Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP: CLI source code

The S2-LP DK package comes with pre-compiled binarys that are used with the GUI application(S2LP_CLI_NUCLEO_L0.hex/ bin). Is the source code available for this CLI? I want to port this to my custom board (containing a STM32G microcontroller), so I ca...

allard by Senior
  • 1867 Views
  • 2 replies
  • 2 kudos

STUSB_NVM_ReadWriteUtility_v1.01

NVM memory read/write CLI utility for STUSBxxxxDescription:Command-line interface utility to program the NVM memory of STUSBxxx products.Thanks to this tool, you can easily automate the process of flashing several devices.It requires a STM32 Nucleo b...

Resolved! BlueNRG-M2: software download and debug

Hi guys. A quick question regarding the swd and debugging on the BlueNRG-M2 module.I have made a little breakout pcb board according to the datasheet: VDD and GND are connected to 3.3V.SWD pins DIO9 and DIO10 har connected to a JLINK (Base Segger), w...

0693W00000ANHMVQA5.png
AWald.2 by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

STEVAL-IDB005V1 and STEVAL-IDB006V1 problems

I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10 so I can't use the GUI to update the Bluetooth stack. Any help would be appreciated.I also have an STEVAL-IDB006V1 that does enumerate but does not ...

RRich.3 by Associate
  • 836 Views
  • 1 replies
  • 0 kudos

There are any way to establish comunication between STMF746 and the PC using the LwIP + RTOS to send and reciving data independently (without handsakeing question/anser)?

I am using the LwIP + RTOS to establish communication between STMF746 and the PC. I was able to send from STM to PC, or from the PC to STM, but I only could be able to do one thing. There are any way to program the STM to be working by 2 thread: one ...

RExpo.1 by Associate
  • 852 Views
  • 0 replies
  • 0 kudos

Resolved! BlueNRG-2 : problem with sleep state

Hello,I have a problem with the bluenrg-2. I'm using a STEVAL-IDB008V2.I measured the current while in different sleep state and here are the results :CPU-HALT : 1.6 mAWAKETIMER : 1.9 mANOTIMER : some nA.The problem is that I'm supposed to have some ...

DActi by Associate II
  • 3342 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.