Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PVilb.1 by Associate II
  • 1123 Views
  • 1 replies
  • 0 kudos

X-Nucleo-IDB05A1 boards problem

I have a few X-Nucleo-IDB05A1 boards, and when I test them on the X-Cube64 board, some work and some don't. So I checked it, and like the attached picture file, the Trace Code and Bulk ID are different.Trace code XN915011 is fine,11540270 doesn't wor...

0693W00000LwlX7QAJ.jpg 0693W00000LwlXbQAJ.jpg
BSalt.1 by Associate III
  • 1307 Views
  • 2 replies
  • 0 kudos

Resolved! Issue in sending ADC value over BLE(BlueNRG-LP)

I am having STEVAL-IDB011V1 board. I am developing the battery profile for that i have refer the ADC_Battery_sensor and BLE_sensorDemo example but the code is stuck in below loop. Please let me know what is the issue in firmware. Is the issue is in A...

Resolved! S2-LP P2P example failing after 2 packets received

I'm not sure if the failure is in tx or rx.The full generated project is attachedtested on dual nucleo-f401RE+S2868A1 boardstest protocol: reset both boards, click few times on blue button of a board, and see it just blink twice on the other board.I ...

Hvan .4 by Associate II
  • 1370 Views
  • 1 replies
  • 0 kudos

i am working on a project where i need to enable BLE as client for that i need to understand a few api and function which are listed below, can anyone help me understand them?

SCH_RegTask( CFG_IdleTask_HciAsynchEvt, TL_BLE_HCI_UserEvtProc );SCH_RegTask( CFG_IdleTask_TlEvt, TL_BLE_R_EvtProc );SCH_RegTask( CFG_IdleTask_Button, LB_App_Button_Trigger_Received );SCH_RegTask( CFG_IdleTask_ConnDev1, LBR_AppConnReq1 ); SCH_RegTask...

MShah by Associate
  • 746 Views
  • 0 replies
  • 0 kudos

Resolved! dma cause error in uart frame, bluenrgLP

Hello community,I configured the uart dma in my project based on the project example USART_TxRx_DMA_Init, and stuck in frame errors, one of the errors is the end of the string seems to be swapped.Sometimes there is no problem the end of the string is...

0693W00000LwbuaQAB.png 0693W00000Lwbt3QAB.png
AndyR1 by Senior
  • 2856 Views
  • 3 replies
  • 0 kudos

How to use BlueNRG GUI v4.2.0

i am not able to connect to hardware on above mention software also get the error as shown in image .i have also followed the UM2058 for steps but after following the step i am not able to connect to hardware.@Sebastien DENOUAL​ @Salvo​ @Salvatore DI...

0693W00000LwfJdQAJ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.