2022-04-06 11:33 AM
I'm not sure if the failure is in tx or rx.
The full generated project is attached
tested on dual nucleo-f401RE+S2868A1 boards
test protocol: reset both boards, click few times on blue button of a board, and see it just blink twice on the other board.
I have no clue where to find the problem, I just see the example is failing fast, and when pushing a button the app think it does send radio frame.
(it goes to: SM_STATE_SEND_DATA, SM_STATE_WAIT_FOR_TX_DONE and back to SM_STATE_START_RX )
stm32cubeide 1.8.0
SUB2G lib+example: 4.2.0
Solved! Go to Solution.
2022-04-06 1:27 PM
it was as stupid as I simply forgot to reduce spi frequency bus from prescaler.
I'm suprised it works a bit at this frequency.
you can delete or move this post as solved :)
2022-04-06 1:27 PM
it was as stupid as I simply forgot to reduce spi frequency bus from prescaler.
I'm suprised it works a bit at this frequency.
you can delete or move this post as solved :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.