Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to reprogram the serial bridge firmware (STM32-F103xx) on the BlueNRG-LP if the serial communication is no longer working?

I was not able to find the answer to this in the QA/Knowledge Base. I understand ST documentation says not to mess with the STM32-F103xx as it comes pre-programmed from the factory. However I have a board whose serial communications between the hos...

JWill.8 by Associate III
  • 3145 Views
  • 7 replies
  • 2 kudos

Resolved! Comunicate RS485 with STR485 on STEVAL-STWINKT1B

I purchased a STEVAL-STWINKT1B development board and inside it has the STR485 chip for RS485 communication.I tried using the cube mx and configured it appropriately (see image 1 attached), enabled uart2, RS485 flowcontrol and then checked that the pi...

JTLGE by Associate II
  • 1834 Views
  • 1 replies
  • 0 kudos

STUSB4500 issue with USB2.0 data with macOS

We have an application where the STUSB4500 is used in conjunction with and STM32L4 family MCU, handling USB2.0 data. So the STUSB provides power (USBPD) and the DP DM lines are routed to the MCU. There is an issue specifically when using a macOS lapt...

RRicci by Associate II
  • 2804 Views
  • 4 replies
  • 0 kudos

Spirit1 mc_state code 0x13

Hi! I'm working with spirit1 module. I'm monitoring internal registers reading them one time per second. After reset mc_state registers C0 and C1 contains values 0x02 and 0x07, what means READY state. I'm trying to put it now in RX mode with command ...

GZeps.1 by Associate
  • 843 Views
  • 0 replies
  • 0 kudos

CubeIDE Error : strange error using git

Hello, I'm using git with my project based on a CubeWL example. After wanting to add this gitignore and delete unnecessary files (i.e. examples that I don't use, but I kept the drivers of course), it doesn't work anymore... ...Git/STM32WL55/STM32Cube...

0693W00000LwxqQQAR.png
LLr.1 by Senior
  • 3993 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.