2022-06-07 12:36 AM
Hello,
anybody can explain to me the difference between the BlueNRG-2 SoC and the BlueNRG-2N co-processor?
Thank you,
Sincerely
Solved! Go to Solution.
2022-06-07 5:07 AM
Hi @malarab ,
BlueNRG-2 is a SoC where you can run your custom fw/application together with BLE stack - Everything running on same cortex-m0. BlueNRG-2 SDK is available here and it includes different code examples
BlueNRG-2N is a network processor, it comes already preflashed and ready to use. We talk about co-processor because in this case it requires an external host microcontroller to execute your application.
BlueNRG-2N is connected to this host microcontroller via SPI or UART. This is ideal solution when you want to add BLE to an existing application or if you hare having a specific microcontroller which is having fetures not supported by a standard BLE SoC.
Regards,
Sebastien.
2022-06-07 5:07 AM
Hi @malarab ,
BlueNRG-2 is a SoC where you can run your custom fw/application together with BLE stack - Everything running on same cortex-m0. BlueNRG-2 SDK is available here and it includes different code examples
BlueNRG-2N is a network processor, it comes already preflashed and ready to use. We talk about co-processor because in this case it requires an external host microcontroller to execute your application.
BlueNRG-2N is connected to this host microcontroller via SPI or UART. This is ideal solution when you want to add BLE to an existing application or if you hare having a specific microcontroller which is having fetures not supported by a standard BLE SoC.
Regards,
Sebastien.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.