2022-07-08 1:15 AM
We use VL53L1X for our product development. Based on the datasheet, the typical operating condition for AVDD is 2.8V. I wonder if we can use a 3.2V for AVDD? If 3.2V
is provided for AVDD, is there any problem that may affect the performance of VL53L1X?
best regards
Dai Sai
2022-07-08 4:49 AM
Hello,
The sensor operating voltage range is [2.6 to 3.5 V], so 3.2V is perfectly suitable to use as long as the voltage regulator is good enough to ensure that the voltage will not be higher than 3.5V. 5% tolerance voltage regulator for example will be fine.
Did you mean 3.3 V or 3.2V, for me the 3.3V voltage is a standard voltage like 2.8V, 1.8V etc ...
Thanks
Julien
2022-07-09 5:37 PM
Dear Julien,
thank you very much for your reply. The SoC we adopted will provide a 3.2V power, it is very good
quality voltage. It will not be over 3.3 in any situation. Based on your information, we will drive VL53L1X
directly with this 3.2V.
best regards
Dai Sai
2022-09-06 4:41 AM
Dear Julien,
I use 3.3V for VL53LX1, but I can not find information for setting the module in 2V8 mode.
I use ultra-lite driver (STSW-IMG009) as driver.
Would you like to tell me how to do in ultra-lite driver (STSW-IMG009) environment?
best regards
Dai Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.