Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X people counting library

Hi,I am using VL53L1X in our cortex-m33 platform.Do you have any library for our cortex-m33 based on your VL53L1X tof sensor for people counting. If yes, please share the library. If the library is not available for our platform, what is the challeng...

Akuma.6 by Associate III
  • 3331 Views
  • 7 replies
  • 0 kudos

Resolved! VL53L5CX Ultra Lite Driver (ULD) - Reflectance Value Format

Hi,I would need a technical information about VL53L5CX Ultra Lite Driver (ULD).Specifically, what is the format of the reflectance value returned by the vl53l5cx_get_ranging_data() function?I am supposing that the format is a percent value expressed ...

MFabb.1 by Associate II
  • 2163 Views
  • 2 replies
  • 0 kudos

VL53L5CX Emitter: 940nm light?

Hi, I would like to know if VL53L5CX emits only signals at this wavelength 940nm or from 900nm to 940 nm, because when I put the sensor in front of a lidar using 905nm, it is clear that the lidar picks up the interference signal from VL53L5CX. If so,...

DWang.7 by Associate III
  • 3111 Views
  • 6 replies
  • 0 kudos

VL6180x at low SPI clock speeds.

I am using a VL6180x with an Atmega8a in a lower-power application. The Atmega8a runs at a clock frequency of 1 MHz. After struggling for a few weeks to get the sensor working, I discovered an issue with the VL6180x. After writing 0x01 to register 0x...

TMout.1 by Associate II
  • 2449 Views
  • 4 replies
  • 0 kudos

How to set 2V8 power mode with VL53L1X ULD API

Dear Sir,We connect VL53L1X to our host that provide 3.3V VDDIO. We will use VL53L1X ULD API as driver for our system. By check VL53L1X ULD API code, I can not find code about setting power mode to 2V8. Would you like to give any information for thi...

DSai.1 by Associate III
  • 1656 Views
  • 2 replies
  • 0 kudos

Operating condition about AVDD of VL53L1X

We use VL53L1X for our product development. Based on the datasheet, the typical operating condition for AVDD is 2.8V. I wonder if we can use a 3.2V for AVDD? If 3.2Vis provided for AVDD, is there any problem that may affect the performance of VL53L1X...

DSai.1 by Associate III
  • 1660 Views
  • 3 replies
  • 0 kudos

about ApiExample in STSW-IMG007

Dear Sir,We are going to port VL53L1X API driver to our threadX environment.We download the en.STSW-IMG007.zip and a document stsw-img007.pdf.The document of API described that there are Api, ApiExample and doc in this package, but there are only A...

DSai.1 by Associate III
  • 1441 Views
  • 2 replies
  • 0 kudos

Can't switch VL53L1 and VL53L1x sensors into threshold mode.

Dear Sirs, I have some problems with VL53L1 and VL53L1X sensors which i'm using in my project.Now i'm trying to figure out how to switch them to different modes and apply different settings in accordance with API manuals and datasheets. I'm also usin...

DBlok.1 by Associate
  • 3705 Views
  • 4 replies
  • 0 kudos