2022-09-05 5:12 AM
Dear Sir,
We connect VL53L1X to our host that provide 3.3V VDDIO. We will use VL53L1X ULD API as driver for our system. By check VL53L1X ULD API code, I can not find code about setting power mode to 2V8. Would you like to give any information for this question?
I wonder if VL53L1X may be broken, when a 3.3V power is given before software initialization.
The datasheet say the default power mode is 1V8.
best regards
Dai Sai
2022-09-06 7:04 AM
Hello,
Over the time, it has been proven that the default power mode at 1.8V is not used.
No need to switch from one mode to another. The VL53L1CX can be used from 1.8V to 3.3V without any problem. You can sent the power to 2.8V before software initialization without any issue.
Best regards
Anne
2022-09-06 3:34 PM
Dear Anne,
Thank you very much for your quick reply for my question.
It's good that we do not need to setup power mode.
best regards
Dai Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.