Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5cx sensor not responding correctly

Hello!I have a VL53L5cx ToF sensor on a X-NUCLEO-53L5A1 shield connected to a Nucleo F401RE and I have run a sample in zephyr and all is okay. I get a successful init and the sensor starts to range correctly:I now have a custom solution using a STM32...

0693W00000Y9TFTQA3.png 0693W00000Y9THoQAN.png 0693W00000Y9TI3QAN.png 0693W00000Y9TIIQA3.png
DOste.2 by Associate
  • 1806 Views
  • 1 replies
  • 0 kudos

is there any vl53l4cx linux software for users?

There are also user folders in the linux drivers of sensors such as vl53l5cx, vl53l1x, but I could not see this folder in the vl53l4cx linux driver and I could not find it anywhere else. Is there software available for users or do we have to create i...

OEdem.1 by Associate
  • 1602 Views
  • 1 replies
  • 0 kudos

Ranging results values for VL53L4CD

Hi,I am getting started with VL53L4CD so as to improve our system under ambient daylight conditions, which is performing poorly due to current sensor VL6180x under such condditions.My application is:Waking up device when target detected closer than 1...

Jhern.1 by Associate II
  • 3228 Views
  • 5 replies
  • 0 kudos

Changing the cross-talk calibration distances for the VL6180X

Hello!So in the project I am working on, we are using ToF sensors (with a cover glass) to accurately measure the distance of a white object within the ranges of 30-70mm. We would like to create a calibration fixture that also falls within these dista...

AGome.7 by Associate II
  • 1770 Views
  • 2 replies
  • 0 kudos