Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X in a tube.. Tips and tricks?.

I like the VL53L1X because the ROI is narrow, and I have seen other posts about a TOF in an opaque tube, but have a few questions still. I get that the beam can be narrowed to 15 degrees, and I have seen that the suggestion is to use matte black i...

CBarr.3 by Associate
  • 1825 Views
  • 1 replies
  • 0 kudos

Initialisation of the VL53L5CX failed.

Hi, I read the question from 'Peter': VL53L5CX driver vl53l5cx_init() fails in the forum and wonder if downloading the firmware was successful. I am using a Rasberry Pi and used the Unosquare.WiringPi, C#.There is no methode to write multiple bytes, ...

BPutt.1 by Associate II
  • 1444 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5CX Offset Calibration

Hi,I noticed that an offset calibration function is missing in the API of the VL53L5CX (like seen before on VL53L1CX). Only the xtalk calibration is available.Is this because all the VL53L5CXs are individually factory offset-calibrated?My assumption ...

MFabb.1 by Associate II
  • 2382 Views
  • 2 replies
  • 0 kudos

Error Message after Start VL53L1X_GUI "Ranging Sensor Failure" ..."SciChart.Chartig3D..SciChart3DSurface" ... Exception

I have Problems to Start the VL53L1X_GUI (STSW-IMG0081.0.0 - R10647), after Installation on different "Win 10 Pro 21H2"-Systems, with or without plugged target board, the error message is always the same: "Ranging Sensor Failure" by calling the c...

JEich.1 by Associate
  • 1582 Views
  • 3 replies
  • 0 kudos

Recently the st has partnership with Metalenz for new technology for tof sensor, Are these new tof sensor available in the market 1.if yes please provide the part number . 2. If no , what is the expected time to be available in the market.

Recently the st has partnership with Metalenz for new technology for tof sensor, Are these new tof sensor available in the market 1.if yes please provide the part number .2. If no , what is the expected time to be available in the market.3 . What is ...

vrast.1 by Associate
  • 1233 Views
  • 1 replies
  • 2 kudos

Am I implementing this liquid level detection right?

I am impementing a water level detection in the sub 1 meter range down to ~50 mm closest distance.My environment is consistently pretty dark concerning visible light. There is no change in time of ambient light.There is very little dynamics in level ...

ABrun.7 by Associate
  • 2377 Views
  • 3 replies
  • 0 kudos