Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question regarding enabling/disabling Crosstalk Compensation

Hello. I am seeking to perform a series of tests to demonstrate the effect of enabling/disabling the cross-talk compensation on the VL6180x ToF sensor. For some context, I'll be setting targets of different reflectance across different distances and ...

AGome.7 by Associate II
  • 1664 Views
  • 1 replies
  • 0 kudos

Using DMA for communication with ToF sensor VL53L7CX

Hello,Standard library for ToF sensors, as far as i know, works in blocking mode and it needs few seconds to initialize sensor and later on to gather all of 64 results. In my project I need to handle other process during this time and using DMA seams...

MŻbik.1 by Associate II
  • 2097 Views
  • 2 replies
  • 0 kudos

VL6180 proximity detection logic output mode

Hi, I would like to know if we can configure GPIO0 or GPIO1 as a logic output mode. In datasheet, we can configure in INT mode. But we need to clear the flag each time we have a value. So we have a wrong value during the clearing. I would like to con...

ELECL.2 by Associate II
  • 1546 Views
  • 1 replies
  • 0 kudos

VL53L4CD getting "stuck" returning the same value

When I run the program, the sensor starts up and is working as expected. Occasionally, the sensor gets "stuck" and just sends the same ranging results. I read that the xshut pin is sensitive and can cause a partial reset of the sensor, putting it in ...

BLiso.1 by Associate II
  • 2664 Views
  • 4 replies
  • 0 kudos

LoRaWAN-End-Node + VL53L4CD, Sleep issue

Hello, I'm using the LoRaWAN-End-Node example on an STM32WL55JC MCU to drive the VL53L4CD sensor.  I would like to use the interrupt pin to get the data from the sensor.what is happening is that once __WFI() in the getting data subroutine is executed...

AElgh by Associate III
  • 1471 Views
  • 2 replies
  • 0 kudos

Resolved! X-CUBE-TOF1 VL53L3CX_SimpleRanging not working

I'm trying to use the new example available on st.com for VL53L3CX_SimpleRanging (available inside X-CUBE-TOF1) is an example application shows how to make ranging with a satellite board (VL53L3CX-SATEL green) connected directly to STM32F401RE withou...

0693W00000AN5I1QAL.png
HElni.1 by Associate II
  • 2076 Views
  • 2 replies
  • 0 kudos