Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Limiting data sent from the VL53L5CX I am trying to upgrade the ultrasonic distance sensors on a Heathkit 2000 robot. Its baud rate is 9600, so it could be overwhelmed by an 8x8 data array sent at 60 Hz.

Is it possible to have a computer ask the sensor for only certain pixels when it is needed?From what is posted by your vendor Sparkfun, the data array can be 4x4 or 8x8, and repetition rate can be 1, 15, or 60Hz. Are these options set by the approxim...

MBres.1 by Associate
  • 3695 Views
  • 4 replies
  • 0 kudos

Resolved! P-NUCLEO-53L8A1

I ordered / received the P-NUCLEO-53L8A1 development kit to evaluate the VL53L8CX ToF sensor.It includes:X-NUCLEO-53L8A1 Time-of-Flight expansion board based on the VL53L8series for STM32 Nucleo• NUCLEO-F401RE development boardCould someone possibly ...

Resolved! VL53L1X offset calibration and xtalk calibration

Hello I want to add a glass to my VL53L1X ToF sensor . How should I calibrate for using with glass?I tried to calibrate with the help of the um2510 pdf (I used VL53L1X_CalibrateOffset and VL53L1X_CalibrateXtalk respectively).  After the calibration w...

MOB1 by Associate II
  • 2475 Views
  • 1 replies
  • 0 kudos

Resolved! Use of the VL53L0X with the nucleo-H7A3ZI-Q ( STM32H7A3ZIT6QU)

For a project i need to add the sensor VL53L0X to a program, i've found the Library for the sensor ( STSW-IMG005 ) i can compil the program with no error , but don't work , i'm pretty sure it's from the adaptation from the library to my STM32, if y...

Dg.1 by Associate
  • 1799 Views
  • 1 replies
  • 0 kudos

SIMPLE RANGE MEASUREMENT WITH VL6180 AND STM32WB55

I'M JUST TRYING TO MEASURE DISTANCE USING VL6180X SENSOR WITH STM32 BUT I COULDN'T SUCCEED.CHECKED THE I2C DEV ADDRESS(0X29),VL6180 SENSOR ID(0XB4).AND JUST USING A FEW FUNCTIONS FROM API LIKE INIT, PREPARE, AND POLL MEASUREMENT. I CANN'T IDENTIFY W...

NASOK.1 by Associate II
  • 2440 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L5CX Target Order Values

When I use vl53l5cx_get_target_order, it returns 2.I assume there are only two values (1 & 2). Does 2 = CLOSEST or Strongest?Thanks.Giri

GRama.2 by Associate III
  • 1558 Views
  • 1 replies
  • 0 kudos

Resolved! Vl53L5CX - cause of stop_ranging() to fail

I am encountering a strange problem on the VL53L5CX sensor. Here is the rundown of my setup:3 sensorseach gets initialised and new i2c address is set so they can run simultaneouslyturn all sensors on and wait for external inputThe external input is s...

ALohr.1 by Associate II
  • 3063 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L0X food oil measurement in metal can

hello.I am trying to measure the level of cooking oil in a metal container using the VL53L0X chip.The length and width of the metal container are 25 cm and the height is 35 cm.Please refer to the picture for detailed measurement environment. However,...

DES.png