Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.
I want to connect four SATEL-53L7CX ToF sensors to a Jetson Orin Nx with an AVerMedia D131 carrier board. The board has a 40-pin expansion header with two i2c buses.I have created a wiring diagram to connect every two sensors to each i2c bus. Each se...
Hi all, first post here!I'm working on a project that I was planning to use the VL53L5CX sensor where it is installed at about 5/6ft above the floor and pointed down at an angle of around 45°. The goal is to be able to calculate the surface of the f...
This is my very first post, so hello all! I got a VL53L5CX sensor from SparkFun and I've been playing around with it in the past few days - it seems to be surprisingly accurate and so far has exceeded my expectations.One thing I'm struggling with is...
Reason for asking is that I need to determine which it is as I would like to make use of the ROI capability of the VL53L1 and my understanding is this is not supported by the VL53L0 range. I have the SATEL eval boards, but can for the life of me not...
We have a product(PCB) in mass production as using VL53L0X.There is a problem with some of our products.We tested before sending customer. There is no problem. But, over time we have received complaints from customers. In this case, We can't communic...
Hi,I'm trying to use VL53L4CX sensor outdoor as people passing counter. Is there any way to extend outdoor range of the sensor or tune detection parameters? Currently i'm getting around 50-60cm in overcast conditions.Damjan
Hello Community,I do agree we don't need to write the code as API is well updated, but to understand my output properly I could really use your help on understanding bits of the histogram loop.if ((pMultiRangingData->StreamCount & 1) == 1) ---> what ...
Hello,I'm in doing a project to measure the distance of my car from the wall. I'm in the software development phase using an ESP32 and a VL53L4CX to measure the distance.I'm using ESPHome to develop the entire thing and due to the reason there is no ...
I read that we can not set spad array size on VL53L4CX chip. What is the purpose of function VL53L4CX_SetUserROI, found in VL53L4CX driver? I tried setting two zones or two user rois but detection doesn’t change.Damjan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.