cancel
Showing results for 
Search instead for 
Did you mean: 

Something Wrong with Calibration of VL53L3CX

LOMO
Associate III

Vl53l3CX works well when i init it with DataInit and StartMeasurement Function,but when i add a OffsetCalibration to its init sequence,it output a distance of 8191 mm,which is obviously wrong .Paraments of calabration function are shown in the  following picture,is there anything wrong.any advice will be appreciated.屏幕截图 2023-10-08 155108.png屏幕截图 2023-10-08 154035.png屏幕截图 2023-10-08 154127.png屏幕截图 2023-10-08 154900.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
LOMO
Associate III

the rangestatus of the first measurement is always 255,use VL53LX_ClearInterruptAndStartMeasurement function get

next normal measurement.

View solution in original post

1 REPLY 1
LOMO
Associate III

the rangestatus of the first measurement is always 255,use VL53LX_ClearInterruptAndStartMeasurement function get

next normal measurement.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.