Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! distance measurement

Hello I want to measure the distance of water in a cylindrical container to the lid of the cylindrical container. I need to find the height of the water by subtracting the measured distance from the height of the cylindrical container. Since there is...

AKULC.1 by Associate II
  • 3005 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L5CX & VL53L1CB resolution

Hello,I can't find the measurement accuracy of the 2 sensors mentioned above in your documentation. Could you please provide me with this information?Thank you.Regards, 

Florian3 by Associate
  • 2208 Views
  • 1 replies
  • 0 kudos

Difference Between A and B Message

I've seen references to various A and B or (even and odd) messages for the ToF sensors.In my application, it turns out that every other measurement is not great, so if I throw out packets based on their message ID count, then I get perfect data but a...

Resolved! VL53L5CX safety for human detection

Hello,I plan to use VL53L5CX to measure the distance between the robot and the user (human) in the walker project. I would like to ask if it is safe or not. Regards,Fehmi.

FKara.3 by Senior
  • 1768 Views
  • 1 replies
  • 0 kudos

Resolved! Device unique ID for VL53L5CX ?

Hello all,does the vl53l5cx ULD API (STSW-IMG023) can expose  a unique device ID for the VL53L5CX ? Something similar to the VL51L1 API function call "VL53L1_Error VL53L1_GetUID(VL53L1_DEV Dev, uint64_t *pUid)"  in the driver SWSW-IMG019 ? Kind regar...

LK by Associate II
  • 3397 Views
  • 6 replies
  • 1 kudos

Resolved! Cover Glass - XTalk Limit (Algorithmn) for various FlightSense Products

Hi all,I'am wondernig about the max XTalk level in kcps which various FlightSense products can compensate. I found only for the new VL53L8CX Sensor a  xtalk compensation limit of 300 kcps - mentioned in application note  AN5939 in section 7 : Guideli...

LK by Associate II
  • 2593 Views
  • 3 replies
  • 2 kudos

Resolved! Gesture Library for VL53L5 linking error for b-u585i-iot02a board: undefined reference to taylor_sqr

Hello to all, I create a new project using STM32CubeMX for the b-u585i-iot02a board. Then I added to the project the software and the library for the gesture recognition STSW-IMG035, specific to M33 processor. Compiling, I have this error:Description...

clemente by Associate III
  • 4060 Views
  • 3 replies
  • 1 kudos

IR080C0-IC09-A066-2 cover window for VL53L1X

I am using cover glass window IR080C0-IC09-A066-2. I want the design to be IP69. Where I can get the information that the cover glass can withstand If it is subjected to high water pressure (10000 kPa) and high temperature(80*C)?

Ali_SE by Associate
  • 2277 Views
  • 1 replies
  • 0 kudos

VD6283 on Arduino UNO

Hello everyone,i bought the X-Nucleo-6283A1 development Board from ST together with an Nucleo-F401RE Developmentboard.I have also installed the GUI and it works ok, the calculation of CCT is not performing correct, but thats ok so far...Now i wanted ...

SBurc.1 by Associate II
  • 3735 Views
  • 6 replies
  • 0 kudos

VL53LX API Compatibility

I ended up accidentally discovering that the VL53LX API is compatible with two different sensors.I'm using this platform implementation for Linuxhttps://github.com/ned14/VL53L3CX_rasppiI have the VL53L3CX but also the VL53L4CD.  I've seen that the VL...