Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CX spad map

Is there any way to get an overview of the 16x16 (time-integrated) SPAD array signals? I would like to see how the VCSEL spot looks on the SPAD matrix. Clearly, this information must be present on the chip itself, as it knows about its optical center...

SCH23 by Associate
  • 2650 Views
  • 3 replies
  • 1 kudos

Resolved! VL6180 AVDD question

Hello,I am planning to use VL6180 sensor in my application which is going to communicate with STM32L071. I would like to ask a question since the specification for the AVDD mentioning about optimal value is 2.8V. Do I need to provide some special LDO...

JacekPieczaba_1-1702313620102.png

SATEL-VL53L8 level conversion

Hi everybody,I have purchased SATEL-VL53L8 package containing 2 breakout boards with VL53L8 ToF ranging sensor, and I encountered a peculiar hardware issue. A breakout board has been connected to an ESP32 dev board (3.3V logic level). I have been try...

milukic_0-1702311151639.png milukic_0-1702312170330.png
milukic by Associate II
  • 3877 Views
  • 6 replies
  • 1 kudos

Resolved! VL53L8CH GUI

Hello,I am interested in the ToF-Sensor VL53L8CH to get access to the histogram data. Is there any Evaluation-GUI to easily try out this sensor and to see the histogram data, similar to the GUI for the VL53L8CX (STSW-IMG041 - VL53L8CX Demo GUI)?Thank...

PhKE by Associate
  • 1846 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L0X: How to narrow the FOV

Greetings Team,Have a question (that may not be so quick). Currently working on a project where I need to detect a tube's length, using the VL53L0X, from ~30 to 200mm. The problem is that the inside dimensions of the tube are 20x11mm, quite tight. I'...

JOsbo.1 by Associate
  • 5313 Views
  • 5 replies
  • 1 kudos

Resolved! How to properly drive the VL53L0X into Sleep mode?

The datasheet mentions putting the sensor into sleep by driving XSHUT low. measuring the power consumption shows that the power is consumed more when I connect XSHUT even when I drive it low by 200 microAmp. The XSHUT is normally pulled-up on the bre...

AElgh by Associate III
  • 8703 Views
  • 14 replies
  • 1 kudos

gesture library in STSW-IMG035

Hello! I am an undergraduate student interested in gesture recognition based on ToF ranging sensors. How to use the gesture library to train a model for the STM32CubeMX project?Is there a tutorial? If possible, could you provide the complete project ...

VL53L3CX with Atmega328pb Xplained Mini

Hi,I am using the VL53L3CX distance sensor for a project and I am wondering if it's possible to create my own library functions. The MCU I am using is the ATmega328PB XPlained Mini from Microchip, which only has 32KB of flash memory. The API library ...

castor by Associate
  • 1969 Views
  • 1 replies
  • 0 kudos