Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CX temperature update

Hi,I was wondering if someone can help me with temperature update on the VL53L4CX.According to UM2931  that describes the temperature update in paragraph 3.5 there is a dedicated function named VL53L4CD_Start_Temperature_Update() and can be used when...

Gabor23 by Associate II
  • 6043 Views
  • 6 replies
  • 1 kudos

Resolved! VL53L5CX Power Consumption

Hello @John E KVAM ,Table 14 in the datasheet shows power consumption in Autonomous as going as low as 4.5 mW, but is this only the AVDD power? or total device power? Because I do measure low power draw at those levels, but only on the AVDD pin (and ...

DBonh.1 by Associate III
  • 7240 Views
  • 8 replies
  • 0 kudos

VL53L8 smalles FoV

Hi,I have a project for which I need to measure a tank level of tanks with a maximum depth of 3 meters. The challenging part is that many tanks have filling tubes with an inner diameter of 50mm but a length of 1000mm worst case. I have made this draw...

bitmap.png
daan by Associate II
  • 2172 Views
  • 2 replies
  • 0 kudos

Resolved! Is the VL53L5CX ToF a good choice, considering all the Time-of-Flight sensors family realized by ST for detecting obstacles below the floor level such as holes or stairs?

Hi community, I would like to understand if the VL53L5CX is a good choice to develop an application to detect holes and stairs. I decided to study them since I was impressed by these things:The FoV of 45 ° horizontally or vertically;The granularity o...

0693W00000LxZHEQA3.png 0693W00000LxZI7QAN.png
VNava.1 by Associate III
  • 3736 Views
  • 5 replies
  • 0 kudos

Resolved! maximum temperature (while not operational) of VL53L0X ToF sensor

Hi everyone, can you provide information on the highest temperature and ambient pressure the VL53L0X Time of Flight (ToF) ranging sensor can handle without being damaged? Note: this is not during operation of the sensor (operating temperature is give...

philipw by Associate II
  • 3251 Views
  • 4 replies
  • 2 kudos

Resolved! VL53L8CH Example code to configure for histogram and get data

I want to use the VL53L8CH in histogram mode to distinguish between multiple reflective surfaces. I found a c-driver package in STSW-IMG043, but no useful example how to initialize the sensor and get data out (over I2C).What I'am looking for:1) initi...

MBaum.7 by Associate III
  • 3322 Views
  • 3 replies
  • 0 kudos

VL53L5CX Bouncing Issue

Hello,Even in the SparkFun product introduction video (2.45-3.00 min),  the representative presentation shows there is some bouncing in the sensor reading. I have also experienced the same bouncing issue. How can we deal with this problem? Regards,Fe...

FKara.3 by Senior
  • 1788 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to get a reading from a VL53L3CX sensor on Zephyr rtos

Hello STM Community team:I'm working  with a vl53l3cx sensor on a custom board with zephyr rtos but i am not able to get a reading.To use the sensor I just modified the zephyr driver for the vl53l1x, on the .c file inside the driver I made the follow...

VL53V1CB calibration

HI,I am using ULD API function VL53L1X_CalibrateOffset() and VL53L1X_CalibrateXtalk() to calibrate the sensor and then I store the parameters in EEprom and everything works fine: with VL53L1X_GetResult() I can see the distance of the object and when ...

Fantalucio_0-1700835373286.png