Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L8CX : firmware loading over SPI fails with timeout

Hello,I'm currently using VL53L8CX with an STM32U535 on a custom PCB.I'm using X-CUBE-TOF1 package.I'm able to identify the sensor with SPI at 2MHz using vl53l8cx_is_alive function.I was able to successfully init and use VL53L8 on U-585I-IOT02A dev b...

josselin_1-1716475677011.png josselin_2-1716475706691.png josselin_0-1716474997218.png
josselin by Associate II
  • 2647 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L8CX changing the data rate

Hi everyone, I am currently using the VL53L8CX for people counting. However, I have encountered an issue where occasionally, changing the data acquisition rate during the data collection process causes a disruption and prevents further data acquisiti...

WeiJia by Associate II
  • 4324 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L0X GPIO1 and ranging sequence

HiI refer to the VL53L0X Datasheet DoclD029104 rev5 page 15 article 2.10 Ranging Sequence.There not a lot descritption in your documentI need to understant how GPIO1 stay down before the sensor pull it up when init/ranging/housekeeping phase is finis...

SCADE by Associate III
  • 1808 Views
  • 1 replies
  • 1 kudos

Resolved! Asking the illumination mode of VL53L8CH.

As far as I know, dToF has two illumination modes. One is spot dToF (iPhone) and the other is flood illumination. Which one is VL53L8CH? Thanks.

Jsc by Associate II
  • 2100 Views
  • 3 replies
  • 3 kudos

Resolved! Please check my observations about AN5894

Are formulas 1-4 correct in AN5894?Segment [AC] is the hypotenuse of triangle ACE, and the angle between segments [AC] and [CE] is half the dihedral angle HFOV. Then formula 1 should have a sine instead of a tangent.If I am right, in the example the ...

TGrod by Associate II
  • 4738 Views
  • 9 replies
  • 0 kudos

Resolved! VL53L8CA Data Sheet & Sample

Hello,VL53L8CA is active product on your product list but i couldn't find a datasheet and sample.I have contacted with my local reseller buying termin is 22 weeks. Before buying i would like to have a datasheet and sample. What is the last situation ...

Tamer by Associate II
  • 6239 Views
  • 10 replies
  • 0 kudos

Resolved! VL53L8xx SPI & daisy-chain support

Hi!I’d like to know if the Vl53L8xx product series support “SPI daisy-chaining” ?For a project, I’ll need few of those, either “straight” along a line segment ( +/- like Neonode’s ZForce sensor bar ), as a “grid”, or as an “arc section” ( that is, a ...

Resolved! VL53L4CX meaning of CalibrationData

Hi,I would like to know the meaning of each data in the L4CX calibration data(VL53LX_CalibrationData_t in API), because there is a lot of data for this IC, and I would like to confirm the status of the calibration from the data.Thank you.

YChen.9 by Associate II
  • 2384 Views
  • 3 replies
  • 1 kudos