Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8CH Evaluation Board Purchase

I am looking to purchase an evaluation board for the VL53L8CH in order to take advantage of the CNH data for potential use in AI models.The below expansion board web page has the below text (Link below) Time-of-Flight expansion board based on the VL5...

VL53L8 with nRF52 DK (nRF52832)

Hello,I've been working with a SATEL-VL53L8 sensor for a while. For this I've used the L4RZI board and now i moved into the nRF52 board for more tests.I've been having trouble trying to implement this. I've tried to use the VL53L0 configuration, (CON...

Lourenco by Associate
  • 1338 Views
  • 0 replies
  • 0 kudos

Resolved! X-NUCLEO-53L7A1 and Nucleo-F429ZI

Hello everyone,I just received my X-Nucleo-53L7A1 board and I'm trying to get it working with my Nucleo-F429ZI. In CubeMX,I've selected my board and the appropriate software pack. For the pin configuration, I followed the example provided for the Nuc...

Miickey by Associate II
  • 3363 Views
  • 3 replies
  • 0 kudos

Resolved! TOF VL53L1 autonomous mode with ambient light

Hello,We are using the VL53L1 sensor in autonomous mode to range data, mostly indoors but sometimes outdoor.Following the Table 3 in UM2133, we use the short distance mode in order to have better ambient light immunity when outdoors.However, in the A...

abdmou by Associate
  • 2218 Views
  • 2 replies
  • 0 kudos

VL53LCX Gesture Recognition for Linux

I have used the VL53LCX Linux driver to operate the ToF sensor on the IMX8M Nano board, and the Linux driver is functioning correctly. However, I am encountering issues with implementing gesture recognition functionality. I have used the gesture reco...

VL6180 part to part variation

Hi all,         What is the part to part variation of ST VL6180 ToF sensor? During testing, we keep the sensor at a distance of 50mm from a retro reflector tape. In a batch of 50 sensors, the readout was from ~ 37 mm to  ~51 mm (expected readout is 5...

Syam by Associate II
  • 2233 Views
  • 3 replies
  • 1 kudos

Resolved! Adding multiple vl53l0x sensors

Hi allI have successfully implemented a single vl53l0x sensor, but wish to add more. I found the "AN4846 Application note Using multiple VL53L0X in a single design" documentation:https://www.st.com/content/ccc/resource/technical/document/application_...

ADP1114 by Associate II
  • 18078 Views
  • 30 replies
  • 1 kudos

Resolved! How to filter multitarget readings on ToF sensor

Hello, We've been developing a tank level monitoring system using these sensors: VL53L4CD (18° FoV)VL53L3CX (25° FoV, multitarget)VL53L4CX (18° FoV, multiobject, multitarget) First question is the definitions and distinctions between the terms multiz...

karlacha by Associate II
  • 5395 Views
  • 4 replies
  • 0 kudos