Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L9CX Data Sheet / exclusion cones

We are designing a lens cover to be used with VL53L9CX. Can you share any more data on the FoV of the time of flight sensor? The attached data sheet on the part page is for a different sensor "VL53L7CX" is there a data sheet for the "...9CX" version?...

atucker_0-1770673355029.png
atucker by Associate
  • 624 Views
  • 3 replies
  • 1 kudos

Resolved! Estimated_reflectance and range_sigma in VL53L5 and L8

I have questions regarding estimated_reflectance and range_sigma in VL53L5 and L8The reflectance: how is it calculated? Is it R=signal_rate_per_spads*depth^2/K? the number_of sapds_enabled seems a useless parameter for a user? Can we know this calibr...

Yunlion by Associate II
  • 374 Views
  • 4 replies
  • 0 kudos

Resolved! VD56G3 camera change the Frame start and frame end

Can you increase the delay between Start and end frame packets.I want to make sure there's enough time for it to be detected with the STM32N6. Registers i've tried to use.  * VSYNC_START_DELAY - is for gpio output* FSYNC_IN_DELAY - not sure what it d...

MyDriver.jpeg

Distance measurement trouble with VL53L0X sensor

Hi, i am a student using the VL53L0X time of flight sensor for a final project. I am having trouble getting the sensor data to settle the measured distance is very jumpy and out by 6 cm when measured with s ruler. how would i calibrate the sensor to ...

Setting MIPI single-lane operation of the STEVAL-66GYMA

Hi, I'm using the image sensor evaluation kit with STEVAL-66GYMAI, STEVAL-EVK-U0I and the PC software of STSW-IMG501 to capture video stream. I would like to change the setting of MIPI lane from default dual-lane to single-lane operation. But, I fail...

OGONJU by Associate II
  • 499 Views
  • 7 replies
  • 0 kudos

Resolved! VL53L9CA Availability

Any way how can I get in touch with ST on availability on this product? We would like to implement this into our devices, a devkit or hardware preview would help, we had previously integrated with the VL53L8 and VL53L5 which the result are good, and ...

Resolved! licenses brightsense camera driver

I'm trying to figure out how to make a driver for your camera. The problem seems to be the licensing. The driver is all GPL which would be fine because with the datasheet i could figure out all the calls i need to make my driver work on a non linux d...

Resolved! Clarification about OPERATION constants in VL53L8CX ULD

Hi, just wondering if these constants (specifically NONE and OR both being 0) in the ULD for VL53L8CX are correct#define VL53L8CX_OPERATION_NONE ((uint8_t)0U) #define VL53L8CX_OPERATION_OR ((uint8_t)0U) #define VL53L8CX_OPERATION_AND ((uint8...

PGibs.1 by Associate II
  • 315 Views
  • 4 replies
  • 0 kudos