Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8CH, VL53L7CH Multi-Sensor Time-of-Flight Fusion

Dear ST, For the ToF sensors supported VL53L8CH or VL53L7CH is it possible to make a hardware that depends on 4 x VL53L8CH or 4 x VL53L7CH integrated to increase the number of zones from 8 X 8 to 16 X 16 ?and if it is possible what would be the limit...

Resolved! Missing declaration of VL53L1X ULD (STSW-IMG009)

Hi everyone,I am a beginner working with the VL53L1X sensor on an STM32F103C8T6 using the STSW-IMG009 (Ultra Lite Driver). I am trying to implement a calibration routine, but I am encountering two specific compilation errors inside my VL53L1X_calibra...

Dn1te by Associate II
  • 254 Views
  • 1 replies
  • 0 kudos

VL53L0X : No ToF sensor laser output.

I am using a VL53L0 ToF sensor.If an interrupt occurs, repeat the measurement using the "VL53L0X_GetRangingMeasurementData" function and the VL53L0X_ClearInterruptMask function.Normally, it operates, but the sensor outputs data that seems to be looki...

Resolved! I3C Error on STSW-IMG506_H5 Example

I connected the VD55G1 promodule on the LS-CAM-I3C and connected it to the NUCLEO-H563ZI.The Display X-NUCLEO-GFX02Z1 is also connected.This is exactly the same configuration from the README.md.I get always an error in "ret = platform_i3c_assign_dyna...

VD55G1-NUCLEO_10.001.jpeg
Noeldi by Associate
  • 292 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX Latched INT feature request

Greetings - I would like to request consideration for a Latched INT option similar to that of the STHS34PF80 sensor (Register: CTRL3 22h). I typically utilize the VL53 with Min/Max threshold values and would like the option to have the INT signal lat...

TPhil.3 by Associate II
  • 251 Views
  • 1 replies
  • 0 kudos

Resolved! VD56G3 camera H front and backporch

Is there a way to change the Horizontal front and backporch?   This is a addon to this question* https://community.st.com/t5/imaging-sensors/vd56g3-camera-change-the-frame-start-and-frame-end/m-p/888134#M6406@Jean_Poire 

VL53L1X spurious readings when nothing is in range

I have an application where I run the VL53L1X in lite ranging mode and short distance mode with a timing budget of 10 ms (100 Hz) as described in AN5263.I recently noticed that on at least one unit (and probably more) the VL53L1X reports a spurious d...