Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L4CX - Temperature Issues (Drift)

Recently, I started a post about drift in the static level measurement using the VL53L4CX. I received some directions to continue the investigation, which I followed. I tested the performance by toggling the XSHUT pin as suggested, but it didn’t work...

Need help configuring VL53L8 firmware

Hello, I’m working on a project where I have a Nucleo F401RE connected to a 53L8A1 expansion board. I’m able to get the histogram plot with the ToF sensor on the expansion board but am wondering if I will still be able to get it if I use an external ...

ay0and0 by Associate II
  • 2069 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX using VL53L4CD ULD

Hi!I've been testing the VL53L4CX sensor with its own API. I want to know if I can use the VL53L4CD ULD on my L4CX sensor and achieve the same performance as if I were using a L4CD ULD on the L4CD sensor. I've read similar questions on this forum reg...

LDMigotto by Associate II
  • 1274 Views
  • 1 replies
  • 2 kudos

Resolved! VL53L8CX SPI doesn't work properly

Hi everyone: I am working on a project with VL53L8CX Time-of-Flight sensor from Pololu. I integrated it with NUCLEO-H755ZI-Q board over SPI interface based on the example and driver provided in the STMicro en.STSW-IMG040 software package. I configure...

pshih_0-1725544500633.png pshih_1-1725544500633.png pshih_2-1725544500633.png
pshih by Associate II
  • 12105 Views
  • 21 replies
  • 1 kudos

Resolved! STM32 VL53L7CX SMART PRESENCE DETECTION

Hii,I am working on a project using the STM32 Smart Presence Detection. In order to run the program and get the detection for the person and get some detection readings which file and what are the steps should I follow? I have extracted the STSW-IM04...

Arun28 by Associate
  • 3089 Views
  • 7 replies
  • 1 kudos

Resolved! STEVAL-CAM-M0I compatible with VD55G0 ?

Can the STEVAL-CAM-M0I evaluation board used together with the VD55G0 promodule? ST's marketing material seems to suggest it can, but looking at the schematics of the STEVAL-CAM-M0I the power rails are turned on in the order VCORE first, then VANA, t...

Bildschirmfoto 2025-04-09 um 21.08.50.png Bildschirmfoto 2025-04-09 um 21.09.39.png
asdfasdf by Associate III
  • 1081 Views
  • 1 replies
  • 1 kudos

Resolved! STEVAL-EVK-U0l : Use as Windows Webcam Device

I have successfully used the STEVAL-EVK-U0l with Windows where I connect the USB cable to my Windows device and interact with it via the free software provided ST, this software being called STSW-IMG501.  I would like to start developing some algorit...

dluka by Associate II
  • 1876 Views
  • 4 replies
  • 2 kudos

VL53L4CD clear interrupt does not clear the interrupt

When calling to clear the interrupt of the sensor I wait for the pin to go HIGH again but it never happens. I follow this flow:set i2c addressset low power configset signal threshold to 5000set sigma threshold to 20set intermeasurment ms to 100 and t...

DrD00m by Associate III
  • 2293 Views
  • 4 replies
  • 0 kudos