Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Poor status above 300mm using VL53L4CD

I'm using a VL53L4CD as a proximity switch but with a user selectable threshold. I began developing on XNUCLEO-53L4A1 on a NUCLEO-F401 but have since migrated to my own pcb using STM32C071. I am having difficulty with poor status reports from the ToF...

Resolved! STSW-IMG037 is not work with Breakout Board

I try  STSW-IMG037 software with  Nucleo STM32-F401RE + Expansion board with VL53L7CX+ two Brakout Boards(VL53L7CX).but it dosen't work. STSW-IMG037 software with  Nucleo STM32-F401RE + Expansion board with VL53L7CX is OK.Soft ver v2.2.29327. and 53L...

k_kondoh by Associate II
  • 2464 Views
  • 7 replies
  • 0 kudos

Resolved! how to distinguish a human with a VL53L8CX :´?

Hallo erveryone, I'd like to know if it's possible to use a VL53L8CX to distinguish between a human and an object and other non-living objects. I've done a little analysis of the data collected by the sensor, motion indication, distances, intensity o...

kgb by Associate III
  • 1360 Views
  • 2 replies
  • 0 kudos

Resolved! Looking for VL53L4ED documentation

Hi everybody. Please help me.  I bought a VL53L4ED sensor and would like to learn how to use it.I have found a number of documents and driver examples, but have been unable to find a document describing the internal registers and their function. (pro...

Brazdil by Associate II
  • 16480 Views
  • 16 replies
  • 1 kudos

VL53L7CX Not outputting data on custom PCB

Hello. I have recently made a custom PCB as a learning project and I have issues with getting data from the sensor. I have used multiple VL53L7CX Satel prebuilt breakout boards and those work fine with my software. I have used both the qwiic python l...

ninja_simen_0-1745863928080.png ninja_simen_3-1745864162680.png

Resolved! Setting up the P-NUCLEO-53L8A1 issue

Hi ST Experts, I am working with the P-NUCLEO-53L8A1 evaluation kit and have followed the user guide to install the necessary software packages and GUI. I was able to detect the STLINK COM port connected to the evaluation board. However, after refres...

STLearner_1-1747799679389.png STLearner_0-1747799346552.png STLearner_2-1747799699226.png
STLearner by Associate III
  • 849 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD soft reset or shutdown

How do you perform a soft reset on the VL53L4CD if XSHUT is not used?  I can't seem to find an example.  I see the VL53L4CD_ULP_SOFT_RESET or VL53L4CD_SOFT_RESET is defined, but I don't know what to write to it.Also, how do you shut the sensor down w...