Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EMVA1288 Datasheets

I am exploring STM image sensors for a new project and am evaluating different options. To make an informed decision, I would like to refer to EMVA1288 datasheets, especially for details on read noise and dark current performance. Could you please le...

Resolved! VL53L7CX SDA stuck at zero

Hi, I am testing the SATEL VL53L7CX board, but the SDA on this board is stuck at zero. I have checked that there are no short cuts and that the pull up is there. Any ideas how to solve this?

Resolved! The interrupt of VL53L4CD cannot be used

I found a problem while using the VL53L4CD. My usual practice is to initialize the VL53L4CD after the terminal is turned on. During subsequent use, I only use Start and Stop to control whether to start ranging.Now it is found that when I stop, the te...

Blue666 by Associate II
  • 3668 Views
  • 9 replies
  • 0 kudos

VD6283 for embedded linux

Hi, I have downloaded the STSW-IMG302_LNX which has this description "Linux driver for VD6283 6-channel ambient light sensor, with flicker extraction expansion application programming interface (API)", I want to compile this driver for my embedded li...

aab1_0-1741187662307.png
aab1 by Associate
  • 1205 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX

I am having trouble with the VL53L7CX recording incorrect measurements after being powered on. Often times the distance if off consistently until I unplug it and plug it back in (The raspberry pi). Sometimes even that will not solve the problem. I ha...

raphiec by Associate
  • 1064 Views
  • 1 replies
  • 1 kudos

Resolved! vl53l8ch ULD driver for SPI interface?

Hello community,I just downloaded ULD driver for vl53l8ch. However it looks only i2c interface is implemented in the driver, no SPI interface related is present. Is there a SPI version of the driver available? or I missed something? Thank you./Roland...

Rolandash by Associate II
  • 1495 Views
  • 4 replies
  • 0 kudos

Resolved! VD56G3 Linux driver cannot find camera

Hi,I have installed the v4l2 driver for the STEVAL-56G3MAI1 camera module on ubuntu 22.04.05 LTS on a RPI CM4. But I am unable to access the module through /dev/video0.I have followed the instructions in the linux start guide fro ST BrightSense but I...

ds2 by Associate II
  • 9397 Views
  • 20 replies
  • 3 kudos

Resolved! Invalid signature error in IPA module for VD56G3

Hello.We're having issues after installing the libcamera package for the VD56G3 sensor from https://www.st.com/en/embedded-software/stsw-img502.htmlThe ST IPA is (apparently) being treated as untrusted and we're being forced into IPA isolation, crash...

estevan by Associate
  • 2102 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L1X Low Range issue

We use the VL53L1X in one of our products and have been doing that for over 2+ years now. As this device is not easily solderable, we have been relying on the Chinese supply of breakout boards used in the hobby market.  Just recently we are facing ra...