2025-07-24 1:00 AM
I use the VL53L1X TOF- Sensor on an Arduino Mega.
With just the Sensors, everything works well.
But when I try to read from Serial1 (and I tried Serial2 and 3 as well) I do not receive any Data from the SerialPort.
Without the Sensors the SerialPorts work well.
I do not undestand, where this comes from. Has anyone some advice for me?
Thanks!!
2025-07-30 2:44 AM
Hi
From your description, seems the issue is more platform realted.
Can you share your test codes and log(if have) of the 3 conditions, then we can debug together.
Br
Zhiyuan.Han
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.