Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X: Interrupt-Pin stays low after first ranging

Hello,I am desperate, have been looking for the cause of a malfunction for quite a long time now.I use the VL53L1X with the ULD API.My code looks like the example code:Enable EN-Pinwait for CheckBootState == okSensorInit (Config like ULD, no changes)...

Karsten1 by Associate II
  • 2822 Views
  • 4 replies
  • 0 kudos

Resolved! VCSEL signals interferences for closed sensors (VL53L1X)

Hello,I am designing a system of multiple VL53L1X sensors placed around a drone. My question is whether two sensors are closed and oriented towards the same direction , is it possible that the VCSEL signal from one could affect the measure computatio...

AAmor.2 by Associate II
  • 1284 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1: What is the data format of histogram_ranging_gain_factor?

UM2133 says the default value of histogram_ranging_gain_factor should be 0.971. When I get the data for VL53L1_gain_calibration_data_t->histogram_ranging_gain_factor, I get an integer "1987". The data type listed in the typedef in vl53l1_ll_def.h is ...

MVand.3 by Associate II
  • 1830 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X API example for STM32

Hi, I included the VL53L0X API from ST in a STM32G4 STM32CubeMX project. Now I need a example of how to use the API to init the VL53L0X and do a simple range measurement. I'm using the Arduino VL53L0X module.

Asantos by Senior
  • 6354 Views
  • 2 replies
  • 0 kudos

VL53L1 can measure the target within 8 meters. However, the VL53L1_Gui(api rev 2432 6.6 build 1) showed "NOT VALID" even if the target stood at about 3 meters.

I was evaluating VL53L1 through X-NUCLEO-53L1A2.The GUI (api rev 2432 6.6 build 1) showed NOT VALID, but I checked the Data Log (.csv) and I found the "trueRange_cm" data was valid. I have a question, which data result is true, GUI or Data Log?Thanks...

TYomo by Associate II
  • 1748 Views
  • 3 replies
  • 0 kudos

Resolved! Vl53L1X ROI Programming

I have a 3 VL53L1X satel boards with me .I started testing it out and am facing some minor issues. I saw in the data sheet that I can program the Region of Interest. I am programming it in arduino. I was hoping if I can get a sample code with the pr...

MBabu.2 by Associate II
  • 3130 Views
  • 3 replies
  • 0 kudos

Multiple VL53L3CX with the same interrupt wire

Hello,I'm looking for using multiple sensors (10 exactly) in my systems. I have two tricky specifications :get measurement frequency of at least 50Hzlimited as best as possible the space of sensors PCBTherefore I have the idea to use a single interru...

AAmor.2 by Associate II
  • 1735 Views
  • 3 replies
  • 0 kudos

noise reduction for VL6180X

Hi,I am using a VL6180X sensor withSYSRANGE__MAX_CONVERGENCE_TIME: 63READOUT__AVERAGING_SAMPLE_PERIOD: 255What are the best settings for minimal noise?Are there any other setting I have to adjust?I also have seen the video https://www.youtube.com/wa...