Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L3CX Bare Driver on Raspberry Pi?

Hi, I'm trying to get the bare driver running in user mode to work on the Pi, because I just need the easiest way to use the VL53L3CX module, and I think the Linux driver is not necessary. I'm not sure how exactly to get the ULD working on a Pi howev...

VBhat.1 by Associate III
  • 1547 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L5CX works as expected when I ask for VL53L5CX_RESOLUTION_4X4. However, when I ask for VL53L5CX_RESOLUTION_8X8 not so much.

The first pixel of each of eight rows seems to provide a good range estimate in mm but the rest of the data is either zero or some huge number that doesn't respond to changes in the field of view. I assumed I would get 64 range estimates as output of...

0693W00000FAaaeQAD.jpg
KWine by Senior
  • 2646 Views
  • 4 replies
  • 0 kudos

VL53L5 Thresholds

Is there any documentation how to setup the various threshold parameters? These are the macros defined in the vl53l5cx_plugin_detection_thresholds.h#define VL53L5CX_DISTANCE_MM            ((uint8_t)1U)#define VL53L5CX_SIGNAL_PER_SPAD_KCPS      ((uin...

BBald.1 by Associate II
  • 1852 Views
  • 3 replies
  • 0 kudos

VL53L1 returns 65XXX values

I have multizone ranging mode enabled along with SHORT distance mode.I am getting a lot of readings with 65XXX values, for example:[8191, 65277, 65243, 65257, 65312, 65267, 65238, 65168, 65241, 65263, 65239, 65211, 65227, 8191, 65217, 65173, 65244][8...

VL53L5CX Examples (9 & 11) using interrupt

I'm using a X-NUCLEO-53L5A1dev board that I have wired up to a Raspberry Pi. I have also wired the interrupt line from dev board (cn-8 pin 3) to the Raspberry Pi GPIO1 (pin 28 on the 40 pin header). In the examples 9 and 11 there is a dummy functio...

BBald.1 by Associate II
  • 1199 Views
  • 1 replies
  • 0 kudos