2022-03-22 2:33 PM
As shown below, the first line is the distance and the rest are histogram data whci I think is same and not correct?
103
-4652409,-2097499426,1344930034,1327221713,525211626,33064954,-17059034,235676156,1093868795,138478570,-1947005701,2044266306,-979944,-1949171152,-370016190,-918125440,-1313692902,250674939,1125191931,138674666,-1594359557,1020856133,-983015,-1596849613,
85
-4652409,-2097499426,1344930034,1327221713,525211626,33064954,-17059034,235676156,1093868795,138478570,-1947005701,2044266306,-979944,-1949171152,-370016190,-918125440,-1313692902,250674939,1125191931,138674666,-1594359557,1020856133,-983015,-1596849613,
80
-4652409,-2097499426,1344930034,1327221713,525211626,33064954,-17059034,235676156,1093868795,138478570,-1947005701,2044266306,-979944,-1949171152,-370016190,-918125440,-1313692902,250674939,1125191931,138674666,-1594359557,1020856133,-983015,-1596849613,
This is the code snippet I am using
VL53LX_GetAdditionalData(VL53L3A2_DEV_CENTER,pAdditionalData);
for (int j=0;j<24;j++){
printf("%ld,", pAdditionalData->VL53LX_p_006.bin_data[j]);
}
printf("\n");
2022-03-25 4:22 PM
There is no way to get the same data if in fact you are ranging. For some reason you stopped ranging.
You should call
VL53LX_GetMeasurementDataReady() - this will stall until the data is ready
Check the RangeStatus to insure you got a good range
VL53LX_GetAdditionalData() this will get the histogram data.
VL53LX_ClearInterruptAndStartMeasurement() - to start the next range.
if your VL53LX_GetAdditionalData() continues to return the same data, you have not completed the next range.
2022-03-27 12:23 PM
I think the problem might lie in me using the VL53L3A2_DEV_CENTER as I think it has the value 0 and not the proprer address which is required? I have trouble finding what to use instead of that. Could you maybe point me in the right direction? I am using the eval board and fr401e board for this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.