Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get proper lux readings from VD6283

I'm working on a mass market application involving VD6283.I run the VD6283 app_lux_cct, and control the sensor using a serial terminal on the PC.The 6 channels are properly displayed along with the lux and cct.However, when I increase or decrease the...

Mvan .18 by Associate II
  • 2126 Views
  • 3 replies
  • 0 kudos

VL53L5CX High current draw in HP idle.

Hello,I have a X-NUCLEO-53L5A1 board wired up with SDA, SCL, 5V, PWR_EN and GND only. The sensor works and current draw is as expected in its ranging and LP idle states. However, when first booted up it will draw a normal 6mA in its HP idle then will...

jspiller by Associate II
  • 1245 Views
  • 1 replies
  • 1 kudos

VL53L4CX integration with esp32 problem

I am trying to measure with the sensor VL53L4CX controlled by an ESP32 (4MB Flash) on ESP IDF. I have installed the drivers STSW-IMG029 v1.2.8 and implemented the I2C functions to read from the sensor, but the ESP32 boot when the I2C read something f...

0693W00000NsHT0QAN.png
Mcabe.1 by Associate II
  • 2938 Views
  • 3 replies
  • 0 kudos

VL53L1X minimum time to to scan from standby

I apologize I have not read ALL of the related documentation but have read enough to feel it may be hard to resolve this question:I would like to employ the VL53L1X to detect object flow, i.e. people, however as someone has already point out it requi...

Tcodd.1 by Associate II
  • 1376 Views
  • 1 replies
  • 1 kudos