Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L4CD repeatability of small measurements

I see from the datasheet that the indoor measurement accuracy at 1-100mm is +/-7mm. I’d like to use the sensor to measure the deflection of a piece of stainless steel, which is used as part of an actuator to hold an object still for measurement. Basi...

VL53L1 Solar Test Method

Hello.I am using the VL53L1.It's fine for indoor lighting.However, in sunlight, the measurable distance becomes shorter.Is there any way to test it similar to this sunlight?Could you please tell me how to test it in relation to sunlight?​thank you.

joh.5 by Associate II
  • 1107 Views
  • 1 replies
  • 0 kudos

What's the meaning of the Reference SPADs calibration? What's the meaning of the number and type of reference SPADs? What happens if VL53L0X_SetReferenceSpads() and VL53L0X_GetReferenceSpads() are not used?

I have used VL53L0X without using VL53L0X_SetReferenceSpads() and VL53L0X_GetReferenceSpads(). The VL53L0X are working well without using them. I found out that some VL53L0Xs have narrower FOV than others and that VL53L0X_SetReferenceSpads() and VL53...

WOh.2 by Associate II
  • 1148 Views
  • 1 replies
  • 0 kudos

Resolved! tap / double-tap detection using VL53L3CX

I would also like to clarify whether there is support for the multi-zone VL53L3CX sensor? Do you have code samples or libraries for tap / double-tap detection using VL53L3CX?

Vandr.1 by Associate II
  • 1420 Views
  • 1 replies
  • 0 kudos

We would like to use the VL6180 sensor in an underwater robot and we would like to know some details about the sensor in order to find the most suitable configuration for our needs.

Is it possible to adjust the LED current ? (increase the current a little bit to compensate for water absorption).Could you give us more details about the WAF? because we've observed a strange behavior during underwater measurements (for targets with...

jmont.2b by Associate
  • 1455 Views
  • 2 replies
  • 0 kudos

Is the VL53L5CX IEC 60825-1:2007 and IEC 60825-1:2014 compliant and harmonized with the DIN EN ? Is there a compliance report available ?

Hello,Next week I have to assemble and demonstrate my project in my local school. My project includes the VL53L5CX-Satel. Does the VL53L5CX compliant with the DIN EN ? Can you provide me a compliance report wich include all the measured limits of the...

MaikH by Associate II
  • 4283 Views
  • 9 replies
  • 0 kudos

Dust free advice - ToF cover glass

During "Discover our latest range of ToF sensors featuring improved short range performance"(28.06.22) it was said you have tip to reduce dust for cover glass. I want to ask about this tip.

KNawa.1 by Associate II
  • 2654 Views
  • 2 replies
  • 0 kudos