2022-07-23 4:43 AM
Dear Sir,
We will develop system with VL53L1X. Now we are going to port the driver for our Thread RTOS. There are several sample version at candidates such as STSW-IMG007
, STSW-IMG009 , STSW-IMG013 and STSW-IMG032. Could you give me some advice for selecting the sample code? which one is better for our case?
best regards
Dai Sai
Solved! Go to Solution.
2022-08-02 4:22 PM
If the ULD API (STSW-IMG009) suites to you, please choose this one. It is simple, small, easy to use.
The full driver STSW-IMG007 is more complete but the simplest driver will do most of what you want.
If you don't need Linux nor Ultra Low Power, you can forget the two others.
Regards
Anne
2022-08-02 4:22 PM
If the ULD API (STSW-IMG009) suites to you, please choose this one. It is simple, small, easy to use.
The full driver STSW-IMG007 is more complete but the simplest driver will do most of what you want.
If you don't need Linux nor Ultra Low Power, you can forget the two others.
Regards
Anne
2022-08-05 5:23 PM
Dear Anne,
Thank you very much for your reply.
Based on your advise, we will port STSW-IMG007 to our RTOS for future
possible function extension.
best regards
Dai Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.