cancel
Showing results for 
Search instead for 
Did you mean: 

Teseo-VIC3D

rasmus_cplace
Associate

Hi

I have some question regarding the Teseo-VIC3D information which I cannot find.

1. The Teseo-VIC3D should have its own asm330 unit which internally is interfaced over SPI, right? 

2. Is it possible to interface the ASM330 as if it where an external hw unit?

3. Or just to get the values?

3a. If yes how often?

3b. and is it calibrated, raw or both values?

4. I can see there are several commands to set uart/nmea port speed
- CDB-ID 102 – NMEA port baud rate setting
- $PSTMCFGPORT on UART

are there any difference in which to use?

 

/Rasmus

1 REPLY 1
GalaxyQuest
ST Employee

Hi Rasmus,

Yes internally ASM330 is interfaced to Teseo-3.

You cannot interface directly to ASM330.

VIC3D outputs the raw sensor values. You can enable this through modifying the CDB setting as follows,

 

$PSTMSETPAR,1228,0x10000000,1  //enables DR messages
$PSTMSAVEPAR   //save values to flash
$PSTMSRR       //save and reset

 

The default value is 100 Hz but you can change it. Please refer to this post,

https://community.st.com/t5/gnss-positioning/accelerometer-data-throughput-or-retrieval-by-request-on-teseo/td-p/769269

These are raw values.

CDB-102 sets the baud-rate whereas the $PSTMCFGPORT sets the type of interface used. If you are looking to change the baud-rate I would change CDB-102 register.

$PSTMSETPAR,1102,0xC //for 460k baurd
$PSTMSAVEPAR
$PSTMSRR   //save and reset for setting to take effect

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.