| Subject | Author | Posted | |
|---|---|---|---|
|
Hi everyone, I'm working on decoding an SBUS signal, which uses an inverted normal UART protocol, ...
| 2024-08-18 8:26 AM | ||
|
Hi,
I have ported the Open Bootloader to the STM32G431 and has flashed it and is able to communic...
| 2024-08-14 5:33 AM | ||
|
Well, I'm developing a system for reading sensors and sending them to a server. I'm using a GSM LT...
| 2024-08-13 8:45 AM | ||
|
I've successfully set up an evaluation project on the STM32U5A9J-DK PCB with a custom 640x480 MIPI/...
| 2024-08-13 7:34 AM | ||
|
I'm currently testing low-power applications on the NUCLEO-U545RE-Q board, which involves using an ...
| 2024-08-13 12:32 AM | ||
|
Hi, I'm using the software EEPROM to save a variable to flash that is being updated during run tim...
| 2024-08-12 5:40 PM | ||
|
I am trying to implement an IAP function on stm32h563 with Keil. I have a bootloader and image A an...
| 2024-08-12 3:41 PM | ||
|
Hello, SDIO 4 bit R/W with 32 bit HC works. When 64 GB XC is used getting error at: SD_PowerON() ...
| 2024-08-12 6:26 AM | ||
|
Hi, I am very new to the matter protocol and seeking to implement a matter protocol for STM32 NUCL...
| 2024-08-11 10:42 PM | ||
|
I am trying to flash and debug my .elf file with the help of openocd and gdb server in UBUNTU . Aft...
| 2024-08-11 11:02 AM | ||
|
Hi there, I am writing a custom video decoding app that process custom stream JPEG frames from USB,...
| 2024-07-30 6:16 AM | ||
|
If you enable Transmission Complete (TC) interrupt flag TCIE in the UART_CR1 register before enabli...
| 2024-07-30 1:30 AM | ||
|
I made a board with spi1 connect a lora module, and the nss pin, I just want to use soft control. B...
| 2024-07-29 4:52 AM | ||
|
Hi all, Currently I am working on a project using STM32U575ZG with both ADC1 and ADC4 enable. 1...
| 2024-07-25 7:10 AM | ||
|
I am working with an STM32F405 and have the I2C1 peripheral set up as a master in standard mode wit...
| 2024-07-25 6:50 AM | ||
|
Good day, Hope you're well. I used CubeMX to setup a PWM timer on the STM32F3 discovery board and ...
| 2024-07-24 7:26 PM | ||
|
Hello, We are using STM32L412RBT6 MCU for our inverter and battery charger application. We are ...
| 2024-07-24 3:33 AM | ||
|
Hello, I have a code snippet where I initialize PSP (stack pointer) to its very first location, an...
| 2024-07-23 11:36 PM | ||
|
Hi everyone, I'm new to STM32. I'm trying to use the STM32C011x4's internal temperature sensor. I'...
| 2024-07-22 12:58 PM | ||
|
Any suggestions as to why power down, then reconnect debugger (JLINK pro) is clearing the ...
| 2024-07-22 8:16 AM |