| Subject | Author | Posted | |
|---|---|---|---|
|
I generated a project using STM32CubeMX, in which I tried to use SDIO and FatFS. However, it doesn...
| 2024-07-20 11:46 PM | ||
|
NUCLEO-F030R8 does not appear in FINDER on Mac
Also the option is missing from list of ports
Ha...
| 2024-07-19 4:13 PM | ||
|
Dear Community. Short Rant (sorry, need to let off some steam): I wonder, why there is not more q...
| 2024-07-17 10:16 AM | ||
|
Hi I'm designing a PCB using the STM32H735 based on the eval kit STM32H735G-DK. On STM32H735G-DK ...
| 2024-07-17 1:19 AM | ||
|
This is new. I've used it in the past and downloaded data with no problem. Yes, I do have netw...
| 2024-07-16 11:53 AM | ||
|
Previously, I had a Raspberry Pi CM4 connected to an existing WebSockets server developed with Djan...
| 2024-07-16 8:38 AM | ||
|
Hello, I have been working on the STM32G030K6T6 with DMX512 and TM1651 display for 8 months, and I ...
| 2024-07-16 5:26 AM | ||
|
Hi everyone, 1, What are the acceptable buffer sizes for the DFSDM PDM mic configuration, give me ...
| 2024-07-15 11:55 PM | ||
|
Hi, I am unable to communicate via i2c with the TLV320AIC3104IRHBR chip, the bus response is always...
| 2024-07-15 2:20 PM | ||
|
Hi there, Iam able to send data to external DAC with SPI DMA timer update on the SPI-2, the proces...
| 2024-07-10 8:59 PM | ||
|
Hello, the reference manual of the STM32G4 Series states, concerning the arbitration of mem2mem tr...
| 2024-07-08 7:55 AM | ||
|
So far, I have the feeling that you can connect ITRx only to TRGO of other timers. I am wonderin...
| 2024-07-05 4:12 AM | ||
|
void tcpsend (char *data)
{
// send the data to the connected connection
netconn_write(conn, data...
| 2024-07-05 12:21 AM | ||
|
I would like to know if it is possible to generate a sweep signal (a sine wave with increasing freq...
| 2024-07-04 11:31 PM | ||
|
I'm developing a vibration and temperature analysis system. To do this, I have developed a sensor ...
| 2024-07-04 6:40 AM | ||
|
Hi, While implementing a single conversion process for the Analog-to-Digital Converter (ADC) via ...
| 2024-07-02 10:09 PM | ||
|
I am making this code which, on an interrupt, is supposed to wake the system from STOP mode, put it...
| 2024-07-02 7:47 AM | ||
|
Hello, After reading the following threads: How to program STM32 Option Bytes with the HAL API - ...
| 2024-06-28 6:12 AM | ||
|
Hi there, I have some question about the deferent about the source code and the lib. For example,...
| 2024-06-27 8:13 PM | ||
|
I am using NUCLEO-G071RB. I use 2 ADC channels: GPIO analog and internal temperature sensor. I conn...
| 2024-06-27 6:00 AM |