| Subject | Author | Posted | |
|---|---|---|---|
|
Hello guys! I have a problem. I need to use HAL_RTCEx_SetSynchroShift function from HAL to modify t...
| 2024-06-26 11:10 AM | ||
|
I found a confusing phenomenon that I found when using STM32G431CBU6 OPAMP3 works in Timer controll...
| 2024-06-26 7:27 AM | ||
|
I am using STM32H5 nucleo board and it is connected with MIC which gives PDM output based on analog...
| 2024-06-26 4:36 AM | ||
|
Hello, I am doing a project on making a car display using STM32H735, but the Display on it is small...
| 2024-06-25 9:45 PM | ||
|
Hello ! I'm new here and I'm new to programming with a big project. I ordered a Nucléo F401RE wit...
| 2024-06-25 2:00 PM | ||
|
At present, when STM32L412 uses the HAL_SPI command to read back the Register, no matter which Regi...
| 2024-06-25 2:20 AM | ||
|
Hi ST tesam, When I use the HAL of STM32C031, I have some trouble about SMBus. Q1:When I use the ...
| 2024-06-24 1:18 AM | ||
|
I want to connect 2 Nucleo F103RB as slave (2 Nucleo slaves) to one master (PC for now) over Modbus...
| 2024-06-23 9:42 PM | ||
|
Hello, I've a project with the STM32G030F6 which the application use in 90% of time the low power ...
| 2024-06-21 1:09 AM | ||
|
I am working on an application using an STM32U5A5 nucleo board with four MEMs PDM output format mic...
| 2024-06-20 11:49 AM | ||
|
I am experiencing an issue with the Dual Boot Bank Swap Boot Loader on my STM32G474RE microcontroll...
| 2024-06-20 7:10 AM | ||
|
Hello,
I have a issue to control IS66WVE4M16EBLL-70BLI with STM32U585AII6.
Although IS66WVE4M16...
| 2024-06-20 1:39 AM | ||
|
The software drives the SPI to drive the RF chip, and I add a 0r resistor to the SPI as shown in Fi...
| 2024-06-19 5:10 AM | ||
|
Hello everyone, I have a stm32l072 microcontroller and an NB exs82 module connected via LPUART. And...
| 2024-06-19 4:53 AM | ||
|
Dear Community Support, Recently, our team acquired an STLINKV3 debugger (MB1440 + MB1441) with...
| 2024-06-17 8:58 PM | ||
|
Hi all, I'm working with STM32F4 disc board, I'm using PB8 and PB9 as interrupt input, those pin s...
| 2024-06-17 6:17 AM | ||
|
I recently started working on a custom board project based on an STM32G070CBT and using the SWD i...
| 2024-06-17 5:10 AM | ||
|
Hi, I try to configure a STM32C031K6 to generate an interupt every seconds using RTC Alarm A (RTC ...
| 2024-06-14 6:56 AM | ||
|
Hi, I have the STM32H753i-EVAL2 and need to boot from TFTP using U-BOOT. As the STM32H743i-EVAL is...
| 2024-06-13 8:53 AM | ||
|
Hi,
I am using Olimex STM32-E407 evaluation board which has STM32F407ZG. I tried Freertos,LWip et...
| 2024-06-13 4:55 AM |