| Subject | Author | Posted | |
|---|---|---|---|
|
We tried to set the OP bytes using the JLink.exe through command line. We tried to enable TZEN and ...
| 2024-10-01 5:40 AM | ||
|
I'm having difficulty writing to STGAP1BS configuration registers. I'm using a Nucleo -G474RE to ...
| 2024-09-26 10:14 AM | ||
|
Hello Community, We have issues with a STM32F407G-DISC1 board. We had the board running in our ca...
| 2024-09-18 9:14 PM | ||
|
Hello, Hello, I am seeking either a ready-to-use or partially implemented driver for the HM01B0 ...
| 2024-09-18 7:57 AM | ||
|
Hi, i start design on G4 and am confused with internal ref in MX. 1. Internal REF for ADC isnt rea...
| 2024-09-18 1:17 AM | ||
|
I am developing a application for Battery based 4G GATEWAY so most of the time I want my micro-cont...
| 2024-09-17 4:49 AM | ||
|
Hello,
I wanted to have SPI with DMA RX, below issues I face:
1. When SPI RX DMA function used...
| 2024-09-15 10:07 PM | ||
|
Hi, I'm trying to apply an Offset on the ADC, I'm using a H743. I'm pretty sure I have the ADC wor...
| 2024-09-15 1:07 PM | ||
|
Hi. I'm trying to configure a wake-up alarm (Alarm A) to wake up (for a test) after 5 minutes, bei...
| 2024-09-13 12:56 PM | ||
|
Hi everyone, long story short is that i'm trying to use the system bootloader capabilities to handl...
| 2024-09-13 1:17 AM | ||
|
Hello, I am using RTC internal wake [10 sec] using the following code: void go_to_sleep(void)
{
...
| 2024-09-12 11:44 PM | ||
|
Hello. In STM32H7S7L8HXH_flash_default_app.ld, it is set to __FLASH_BEGIN = 0x08000000, In STM3...
| 2024-09-12 10:25 PM | ||
|
Hi, the platform is STM32U57X Question: The variable is in the non secure area of SRAM. Why can...
| 2024-09-12 4:30 PM | ||
|
I am using STM32CubeH7 from GitHub (the latest commit is here). In stm32h7xx_hal_nand.c, I found so...
| 2024-09-09 5:05 AM | ||
|
As I am working on the stm32G474VETx with LQFP100 packing. For master and slave, I am using same ty...
| 2024-09-04 1:32 AM | ||
|
I am using stm32f4 for lwip ethernet It works nice with my custom monitoring program, hercules ...
| 2024-09-03 9:35 PM | ||
|
@Erwan SZYMANSKI I am trying to establish SPI communication between two STM boards: the Nucleo G4...
| 2024-09-03 6:05 AM | ||
|
I have a project using all custom code (not HAL) in which I have two 6 byte SPI DMA transactions ru...
| 2024-08-28 1:24 PM | ||
|
Hi As i am using one of TIM8 input for external BKIN pin, to detect fault for PWM shutdwon. But ...
| 2024-08-23 1:10 AM | ||
|
Regarding the KNX TP, I tested the STKNX evaluation board and my board which have ST-KNX chip then ...
| 2024-08-20 4:25 AM |