2019-08-06 9:10 AM
Hello,
When I create a new project in CubeMX for the STM32H747I-DISCO board, I cannot see the X-CUBE-AI package when I click on "Additional Software". Is it because this board has 2 cores Cortex-M7 and M4? Somehow we need to specify on which core the network should run?
In the user manual of FP-AI-VISION1 (UM2611: https://my.st.com/content/ccc/resource/technical/document/user_manual/group1/a0/53/9b/b7/f9/b5/4a/6f/DM00630755/files/DM00630755.pdf/jcr:content/translations/en.DM00630755.pdf), it is written that:
"For users having selected dual-core MCUs for their application but running it on the Cortex®-M7 core only: when dual-core MCUs like the STM32H747 are not supported by the STM32CubeMX tool, they must select a single core MCU like the STM32H743 to be able to generate the code for the Cortex®-M7 core."
So, if I generate an X-CUBE-AI project in CubeMX for, let's say, the STM32H743I-EVAL2 or STM32H743I-EVAL board, would that project compile and work on the STM32H747I-DISCO as well, without any other modification? This seems counter-intuitive to me since the EVAL board contains more features than the DISCO one.
Should I select an MCU (STM32H743xx) instead of an EVAL board, but which one would be the best? I would still need to use the LCD screen (as well as the external Flash memory and RAM) of the H747-DISCO board for my project.
Thank you and kind regards
Solved! Go to Solution.
2019-08-09 9:33 AM
>>..would that project compile and work on the STM32H747I-DISCO as well, without any other modification?
Usually no, what one might consider is making a simple shell project on the prefered target, and then merge in the non-platform specific portions
2019-08-09 8:51 AM
Hello,
Dual-core STM32H7xx products (ex: STM32H747) are not supported by the X-CUBE-AI package at the moment.
So if you want to use X-CUBE-AI package in order to generate neural network code running on the Cortex-M7 core of the STM32H747, you have to select a single core STM32H7xx product (ex: STM32H743).
In X-CUBE-AI package: if you have selected application SystemPerformance or Validation, you need to perform the following changes in order to be able to run the application on the STM32H747-DISCO board:
Best Regards,
Julien.
2019-08-09 9:33 AM
>>..would that project compile and work on the STM32H747I-DISCO as well, without any other modification?
Usually no, what one might consider is making a simple shell project on the prefered target, and then merge in the non-platform specific portions
2020-12-13 10:25 PM
Just curious, how do you init the GPIO on CubeMX for STM32H747I-DISCO? I have the problem in the link below.
https://community.st.com/s/question/0D53W00000NUOGLSA5/cubemx-gpio-not-initialized-in-stm32h747disco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.