cancel
Showing results for 
Search instead for 
Did you mean: 

ST Edge AI Developer Cloud Benchmark not working with STM32F746G-DISCO

mimik
Associate II

Hello! I am working with the developer cloud to benchmark some models' inference speed in a controlled environment. It was working well for the STM32F746G-DISCO board until a couple of days ago, when it just kept saying that my model has a measured inference time of "undefined ms." 

 

mimik_0-1750439169366.png

 

I was wondering if this issue was known and whether it was possible to benchmark the inference time of my model locally on my board with the same environment as the developer cloud. I am aware of the local benchmarking tool in the ModelZoo services, but it seems to only give the estimated memory footprints, not the inference time.

Thank you! 

 

1 ACCEPTED SOLUTION

Accepted Solutions
hamitiya
ST Employee

Hello,

Could you please retry  and see what happens on your end ? 

I was able to reproduce the issue and after an update it is now unstuck.

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
hamitiya
ST Employee

Hello,

Is it possible to share the version you used as well as the model ?

 

Best regards

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thank you for the reply. This error has occurred to me for every model I've tried so far. A model that I have confirmed this error to happen with is the "st_yolo_x_nano_192_0.33_0.25_int8_object_detection_COCO_2017_Person.tflite" in the ModelZoo. The version of ST Edge AI that I used is 2.1.0-20194 329b0e98d, but I also tested it on 2.0.0-20049, and it also did the same thing. Everything was working with the same version 2.1.0-20194 329b0e98d for me on the 18th.

I get the following output from validation: 

ST Edge AI Core v2.1.0-20194 329b0e98d
Setting validation data...
 generating random data, size=1, seed=42, range=(0, 1)
   I[1]: (1, 192, 192, 3)/float32, min/max=[0.000006, 0.999992], mean/std=[0.499628, 0.288319]
    c/I[1] conversion [Q(0.00392157,0)]-> (1, 192, 192, 3)/uint8, min/max=[0, 255], mean/std=[127.405409, 73.521879]
    m/I[1] conversion [Q(0.00392157,0)]-> (1, 192, 192, 3)/uint8, min/max=[0, 255], mean/std=[127.405409, 73.521879]
 no output/reference samples are provided
Creating c (debug) info json file C:\Users\aiprod\AppData\Local\Temp\benchmark-ai-output-directory-c6e629df-136f-4317-a600-fa5198b4289c\network_c_info.json
 Exec/report summary (validate)
 ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
 model file         :   C:\Users\aiprod\AppData\Local\Temp\benchmark-ai-project-directory-6fd50282-ef8e-40db-906e-1e8bfffe007a\STM32F746G-DISCO\st_yolo_x_nano_192_0.33_0.25_int8_object_detection_COCO_2017_Person.tflite   
 type               :   tflite                                                                                                                                                                                               
 c_name             :   network                                                                                                                                                                                              
 compression        :   lossless                                                                                                                                                                                             
 options            :   allocate-inputs, allocate-outputs, multi-heaps                                                                                                                                                       
 optimization       :   balanced                                                                                                                                                                                             
 target/series      :   stm32f7                                                                                                                                                                                              
 memory pool        :   C:\Users\aiprod\AppData\Local\Temp\benchmark-ai-project-directory-6fd50282-ef8e-40db-906e-1e8bfffe007a\STM32F746G-DISCO\.ai\mempools-board.json                                                      
 workspace dir      :   C:\Users\aiprod\AppData\Local\Temp\benchmark-ai-workspace-directory-56e8e5d6-0130-47f9-a2f7-d9ff14cc64c6                                                                                             
 output dir         :   C:\Users\aiprod\AppData\Local\Temp\benchmark-ai-output-directory-c6e629df-136f-4317-a600-fa5198b4289c                                                                                                
 model_fmt          :   sa/ua per tensor                                                                                                                                                                                     
 model_name         :   st_yolo_x_nano_192_0_33_0_25_int8_object_detection_COCO_2017_Person                                                                                                                                  
 model_hash         :   0xac32a7b489150a917c95ccf44349fb1f                                                                                                                                                                   
 params #           :   889,394 items (891.18 KiB)                                                                                                                                                                           
 ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
 input 1/1          :   'serving_default_input_10', uint8(1x192x192x3), 108.00 KBytes, QLinear(0.003921569,0,uint8), activations                                                                                             
 output 1/3         :   'conversion_145', f32(1x6x6x6), 864 Bytes, activations                                                                                                                                               
 output 2/3         :   'conversion_97', f32(1x24x24x6), 13.50 KBytes, activations                                                                                                                                           
 output 3/3         :   'conversion_121', f32(1x12x12x6), 3.38 KBytes, activations                                                                                                                                           
 outputs (total)    :   0 Bytes                                                                                                                                                                                              
 macc               :   112,230,814                                                                                                                                                                                          
 weights (ro)       :   912,572 B (891.18 KiB) (1 segment) / -2,645,004(-74.3%) vs float model                                                                                                                               
 activations (rw)   :   166,316 B (162.42 KiB) (1 segment) *                                                                                                                                                                 
 ram (total)        :   166,316 B (162.42 KiB) = 166,316 + 0 + 0                                                                                                                                                             
 ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
 (*) 'input'/'output' buffers can be used from the activations buffer
  Memory-pools summary (activations/ domain)
  --------------------- -------- -------------------------- --------- 
  name                  id       used                       buffer#   
  --------------------- -------- -------------------------- --------- 
  POOL_0_RAM            0        162.42 KiB (68.8%)         295       
  POOL_EXTERNAL_SDRAM   unused   -                          0         
  weights_array         2        891.18 KiB (91257200.0%)   228       
  --------------------- -------- -------------------------- --------- 
  Warning: ['POOL_EXTERNAL_SDRAM'] memory pool is not used
Running the TFlite model...
Running the ST.AI c-model (AI RUNNER)...(name=network, mode=TARGET)

INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
hamitiya
ST Employee

Hello,

Thanks for your reply.

This output seems incomplete, it looks like the execution failed unexpectedly at the end. Also, it does not happen on other boards

I am investigating the issue.

 

For your question:

> "whether it was possible to benchmark the inference time of my model locally on my board with the same environment as the developer cloud"

You can perform the same kind of action using X-CUBE-AI embedded in STM32CubeMX, using the action "Validate on target"

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
hamitiya
ST Employee

Hello,

Could you please retry  and see what happens on your end ? 

I was able to reproduce the issue and after an update it is now unstuck.

 

Best regards,

Yanis


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi!

Yes, Ive tried it on some of my models and everything works now. Thank you so much!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.