2020-10-05 12:24 AM
The standard way to generate a header file with MLC register settings is to generate from decision-tree .txt file (exportet from WEKA or python).
In our project we want to avoid tool interaction.
The register settings (ucf or header file) should be generated by a script (python....).
Is there a way without user interaction to create the register settings from (weka) decision trees?
regards
Hari
2020-10-05 9:58 AM
Hi @HFenz ,
currently you have to upload the decision tree from Weka to Unico-GUI, as described in this step-by-step online tutorial.
However, ST is working for a tool-free script (should be in python, or a C library for CubeMX).
I'll get back to you in case of recent updates.
-Eleon
2020-10-05 10:21 PM
Hi Eleon,
Thank you for the answer.
A python script would be great.
Thanks
Hari
2020-10-19 1:51 AM
Hi @HFenz ,
You can for now find HERE a python script example (not an entire project, but could be seen as a basis to start before a full Python project routine) containing some code lines to be used as example for generating a decision tree with Python, through the scikit package. The scripts are available both as Jupyter notebook (.ipynb) and as common Python scripts (.py). The example shows how to generate a decision tree file (dectree.txt) starting from an ARFF file (test.arff).
-Eleon
2021-07-15 11:46 PM
Hi @Eleon BORLINI ,
Any update on the tool-free script/code to MLC process a decision tree to a UCF file?
And is there any detailed MLC UCF documentation with worked examples like the UCF examples in AN5273 "LSM6DSOX: Finite State Machine" (section 8)?
Thanks,
Brendon
2021-07-16 1:39 AM
Hi Brendon @Community member ,
finally we could be close to make open the (already) available scripts, as you can see from this thread from last webinar.
Please look for updates on ST GitHub webpage.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.