2025-08-01 3:39 AM
Hello,
im trying to convert a .tflite model (encoder-decoder model, with only supported layers by stedgeai) to C-code to use it in my STM32CubeIde project.
When using the command:
/opt/ST/STEdgeAI/2.1/Utilities/linux/stedgeai generate --model model.tflite --target stm32n6 --st-neural-art
I'm getting the following error output, im not really getting my head around:
ST Edge AI Core v2.1.0-20194 329b0e98d
WARNING: gemm_0 is not quantized
WARNING: nl_0_nl is not quantized
WARNING: gemm_1 is not quantized
WARNING: nl_1_nl is not quantized
WARNING: gemm_2 is not quantized
WARNING: nl_2_nl is not quantized
WARNING: reshape_3 is not quantized
WARNING: gemm_4 is not quantized
WARNING: nl_5 is not quantized
WARNING: reshape_6 is not quantized
>>>> EXECUTING NEURAL ART COMPILER
/opt/ST/STEdgeAI/2.1/Utilities/linux/atonn -i "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_output/gcode_model_OE_3_2_0.onnx" --json-quant-file "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_output/gcode_model_OE_3_2_0_Q.json" -g "network.c" --load-mdesc "/opt/ST/STEdgeAI/2.1/Utilities/configs/stm32n6.mdesc" --load-mpool "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/my_mpools/stm32n6-app2_STM32N6570-DK.mpool" --save-mpool-file "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/stm32n6-app2_STM32N6570-DK.mpool" --out-dir-prefix "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/" -O3 --all-buffers-info --mvei --cache-maintenance --Oalt-sched --native-float --enable-virtual-mem-pools --Omax-ca-pipe 4 --Ocache-opt --Os --enable-epoch-controller --output-info-file "c_info.json"
>>> Shell execution has FAILED (returned code = 1)
$ /opt/ST/STEdgeAI/2.1/Utilities/linux/atonn -i /local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_output/gcode_model_OE_3_2_0.onnx --json-quant-file /local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_output/gcode_model_OE_3_2_0_Q.json -g network.c --load-mdesc /opt/ST/STEdgeAI/2.1/Utilities/configs/stm32n6.mdesc --load-mpool /local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/my_mpools/stm32n6-app2_STM32N6570-DK.mpool --save-mpool-file /local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/stm32n6-app2_STM32N6570-DK.mpool --out-dir-prefix /local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/ -O3 --all-buffers-info --mvei --cache-maintenance --Oalt-sched --native-float --enable-virtual-mem-pools --Omax-ca-pipe 4 --Ocache-opt --Os --enable-epoch-controller --output-info-file c_info.json
saving memory pool description "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/stm32n6-app2_STM32N6570-DK.mpool"
Error: optimize round /home/atonci/ci/atonci/workspace/release_STAI_21/onnx_backend/onnx_passes/transform_gemm_fc_into_conv.cc:201: runTransform: Assertion `(b_shape.size() == 1) || ((b_shape[0].dim == M) || b_shape[0].dim == N)` failed.
Warning: Missing Quantization info for Gemm_1_weights; will consider Gemm_1_weights as a native Float
Warning: Missing Quantization info for Gemm_1_weights; will consider Gemm_1_weights as a native Float
Warning: Missing Quantization info for Gemm_3_weights; will consider Gemm_3_weights as a native Float
Warning: Missing Quantization info for Gemm_3_weights; will consider Gemm_3_weights as a native Float
Warning: Missing Quantization info for Gemm_5_weights; will consider Gemm_5_weights as a native Float
Warning: Missing Quantization info for Gemm_5_weights; will consider Gemm_5_weights as a native Float
NOT all epochs mapped on epoch controller: num_epochs=11 num_mapped_epochs=2 num_blobs=2
<<<
E103(CliRuntimeError): Error calling the Neural Art compiler - ['', 'saving memory pool description "/local/projekte/Uni/Masterarbeit/EmbeddedModelsSt/gcode_prediction_dataset/gcode_prediction_model/STM_friendly_LSTM_model/st_ai_ws/neural_art__network/stm32n6-app2_STM32N6570-DK.mpool"', '', 'Error: optimize round /home/atonci/ci/atonci/workspace/release_STAI_21/onnx_backend/onnx_passes/transform_gemm_fc_into_conv.cc:201: runTransform: Assertion `(b_shape.size() == 1) || ((b_shape[0].dim == M) || b_shape[0].dim == N)` failed.', '', 'Warning: Missing Quantization info for Gemm_1_weights; will consider Gemm_1_weights as a native Float', 'Warning: Missing Quantization info for Gemm_1_weights; will consider Gemm_1_weights as a native Float', 'Warning: Missing Quantization info for Gemm_3_weights; will consider Gemm_3_weights as a native Float', 'Warning: Missing Quantization info for Gemm_3_weights; will consider Gemm_3_weights as a native Float', 'Warning: Missing Quantization info for Gemm_5_weights; will consider Gemm_5_weights as a native Float', 'Warning: Missing Quantization info for Gemm_5_weights; will consider Gemm_5_weights as a native Float', 'NOT all epochs mapped on epoch controller: num_epochs=11 num_mapped_epochs=2 num_blobs=2']But when im using the stedgeai generate command without the --st-neural-art parameter the conversion works and i get the network.c/h files, but im missing the "network_atonbuf.xSPI2.raw" file, which i think is needed for using the model within the application (correct me if im wrong and the network.c/h files are enough)?
So my question is: Can i use the converted C-code of my tflite model, that i generated using stedgeai generate without the --st-neural-art paramter and without the "network_atonbuf.xSPI2.raw" file?
If any further information is needed, feel free to let me know!
Kind regards
Solved! Go to Solution.
2025-08-01 5:23 AM - edited 2025-08-01 5:23 AM
Hello @lyannen,
The --st-neural-art is to use the NPU.
Without it is a running the model only on the MCU, or said differently only with SW epoch.
But yes it works.
I am not sure what the meaning of your error is exactly.
All I can say is that in any case, for the NPU to be used to do the calculation, layers in your model must be in int8.
In short:
no --st-neural-art -> MCU
not quantized int8 -> MCU
else NPU if the layer is supported or potential SW fallback (MCU)
You can find all the documentation here:
https://stedgeai-dc.st.com/assets/embedded-docs/index.html
In particular for the NPU in the section: Neural-ART accelerator™ target
Have a good day,
Julian
2025-08-01 5:23 AM - edited 2025-08-01 5:23 AM
Hello @lyannen,
The --st-neural-art is to use the NPU.
Without it is a running the model only on the MCU, or said differently only with SW epoch.
But yes it works.
I am not sure what the meaning of your error is exactly.
All I can say is that in any case, for the NPU to be used to do the calculation, layers in your model must be in int8.
In short:
no --st-neural-art -> MCU
not quantized int8 -> MCU
else NPU if the layer is supported or potential SW fallback (MCU)
You can find all the documentation here:
https://stedgeai-dc.st.com/assets/embedded-docs/index.html
In particular for the NPU in the section: Neural-ART accelerator™ target
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.