2019-01-04 1:04 AM
Hello,
I have built LED blinky test program in SPC560B-DIS eval, I am setting and clearing LEDs in eval bord. I have introduced delay "osalThreadDelayMilliseconds(500);" between set and clear.
I have used below code for my application, but it throws build error please find attached build error. Please guide to fix the error,
Note if I am commenting line "stm_lld_start(&STMD1,stm0_config);" starts working. but if including throws build error
#include "components.h"
#include "stm_lld_cfg.h"
int main(void)
{
componentsInit();
/* Enable Interrupts */
irqIsrEnable();
/* Activates STM0 Driver */
stm_lld_start(&STMD1,stm0_config);
/* Enable channels and start global counter */
stm_lld_enable(&STMD1);
for (;;)
{
pal_lld_setpad(PORT_C, PIN_GPIO34_LED);
osalThreadDelayMilliseconds(500); // Delay 500 ms
pal_lld_clearpad(PORT_C, PIN_GPIO34_LED);
osalThreadDelayMilliseconds(500); // Delay 500 ms
}
}
Solved! Go to Solution.
2019-02-07 2:03 AM
Hello Nanda ,
You have forgotten to put the call back associated (Cf Demos)
in your main.c
/*stm0 channel 0 callback*/
void cb_stm0_ch0 (void){
uint8_t message[]= "STM0 Channel 0 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 1 callback*/
void cb_stm0_ch1 (void){
uint8_t message[]= "STM0 Channel 1 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 2 callback*/
void cb_stm0_ch2 (void){
uint8_t message[]= "STM0 Channel 2 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 3 callback*/
void cb_stm0_ch3 (void){
uint8_t message[]= "STM0 Channel 3 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}Best regards
Erwan
2019-01-10 2:03 AM
Hello ,
1) you have to configure the components like the application
SPC560BCxx_RLA STM Test Application
2) Put the good clock for B Discovery
3) Regenerate
4) Compile
Best regards
Erwan
2019-01-11 12:19 AM
Hello Erwan,
Thanks for you reply,
I had closely followed the example, i.e. the SPC560BCxx_RLA STM Test Application, I couldn't find anything, I have generated the files successfully but compiling the files gives the error especially object file linking step step.
Thanks,
Anand
2019-01-11 6:37 AM
Hello Nandan ,
Could you send me your installation details ?
Best regards
Erwan
2019-01-15 9:58 PM
Dear Erwan,
Thanks for your prompt reply ,
Please see attached installation details for your reference. hope you can help me out with the problem.
please guide if anything more to be installed.
Thanks in Advance
Anand
2019-01-21 8:22 PM
2019-02-07 2:03 AM
Hello Nanda ,
You have forgotten to put the call back associated (Cf Demos)
in your main.c
/*stm0 channel 0 callback*/
void cb_stm0_ch0 (void){
uint8_t message[]= "STM0 Channel 0 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 1 callback*/
void cb_stm0_ch1 (void){
uint8_t message[]= "STM0 Channel 1 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 2 callback*/
void cb_stm0_ch2 (void){
uint8_t message[]= "STM0 Channel 2 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}
/*stm0 channel 3 callback*/
void cb_stm0_ch3 (void){
uint8_t message[]= "STM0 Channel 3 expired!\r\n";
while (sd_lld_write(&SD1,message,(uint16_t)(sizeof(message)/sizeof(message[0]))) == SERIAL_MSG_WAIT){}
}Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.