2022-12-13 5:21 AM
I am currently working on a project where I am using the serial communication. I am using an AEK-MCU-C4MLT1, with SPC5 studio on a windows PC. In particular, I am capable to transmit data but not to receive data. I tried also by enabling the interrupt, either for the transmission and the reception, and I found out that the program enters in the interrupt each time I call the function "sd_lld_read", even if I send no data externally (from docklight). By sending data from docklight, and looking at the rx_buffer I am not able to read anything.
I attach the relevant part of the code here:
int main(void) {
/* Initialization of all the imported components in the order specified in
the application wizard. The function is generated automatically.*/
componentsInit();
/* Uncomment the below routine to Enable Interrupts. */
irqIsrEnable();
sd_lld_start(&SD1,&serial_config_UART);
sd_lld_read(&SD1, (uint8_t*)aux_rx, 1000);
memset(aux_rx,0,sizeof(aux_rx));
/* Application main loop.*/
for ( ; ; )
{
sprintf(aux_tx,"ATE1\r\n");
sd_lld_write(&SD1,(uint8_t *)aux_tx, (uint16_t)(strlen(aux_tx)));
osalThreadDelayMilliseconds(5000);
}
void rxreceive(SerialDriver *sdp)
{
(void)sdp;
}
void txreceive(SerialDriver *sdp)
{
(void)sdp;
pal_togglepad(PORT_F,10);
}
Do you have any idea of what do I have to do in order to receive data and correctly read data? Do you know if I have to call another function in the interrupt?
Thanks in advance,
Simone
Solved! Go to Solution.
2022-12-15 6:18 AM
I managed to resolve the issue by replacing the original "spc5xx_serve_rxi_interrupt" driver (inside serial_lld.c) with this one:
static void spc5xx_serve_rxi_interrupt(uint32_t isdp) {
SerialDriver *sdp = (SerialDriver *) isdp;
uint16_t sr = sdp->linflexlp->UARTSR.R;
sdp->linflexlp->UARTSR.R = (uint16_t)(SPC5_UARTSR_NF | SPC5_UARTSR_DRF | SPC5_UARTSR_PE0);
if ((sr & SPC5_UARTSR_DRF) == SPC5_UARTSR_DRF) {
if(sdp->config->api_mode != SPC5_LIN_API_MODE_BUFFERED_IO) {
*sdp->rx_buf = (uint8_t)sdp->linflexlp->BDRM.B.DATA4;
//sdp->rx_buf++; // opistara 2021-02-17
sdp->linflexlp->UARTSR.R = (uint16_t)SPC5_UARTSR_RMB;
//sdp->rx_len--; // opistara 2021-02-17
sdp->rx_len = 0; // opistara 2021-02-17
if (sdp->rx_len == 0UL) {
//sdp->linflexlp->UARTCR.B.RXEN = 0; // opistara 2021-02-17
//sdp->linflexlp->LINIER.B.DRIE = 0; /* Interrupts disabled. */ // opistara 2021-02-17
if (sdp->linflexlp->UARTCR.B.TXEN == 0UL) {
sdp->linflexlp->LINIER.R &= ~((uint16_t)(SPC5_LIN_INTERRUPTS));
}
/* Call the related callback.*/
if (sdp->config->rx_end_cb != NULL){
sdp->config->rx_end_cb(sdp);
}
SPC5_LIN_RX_DONE(sdp);
}
} else {
*sdp->rx_write_ptr = (uint8_t)sdp->linflexlp->BDRM.B.DATA4;
sdp->rx_write_ptr++;
if (sdp->rx_write_ptr == sdp->rx_end_ptr) {
sdp->rx_write_ptr = sdp->rx_buffered_io;
}
if (sdp->rx_write_ptr == sdp->rx_read_ptr) {
sdp->rx_read_ptr++;
if (sdp->rx_read_ptr == sdp->rx_end_ptr) {
sdp->rx_read_ptr = sdp->rx_buffered_io;
}
}
}
}
}
and it worked very well for me.
Regarding the configuration "serial_config_UART", I used this one:
SerialConfig serial_config_UART = {
115200,
SD_MODE_8BITS_PARITY_NONE,
SPC5_LIN_API_MODE_ASYNCHRONOUS,
tx_callback,
rx_callback,
FALSE,
NULL,
0,
NULL
};
I hope that this will help you!
Regards,
Simone
2022-12-13 8:53 AM
Hello,
would you please show me your structure "serial_config_UART" ?
Best Regards.
2022-12-14 8:11 AM
Hi,
thanks for the response,
I managed to resolve the issue by modifying the driver of spc5xx_serve_rxi_interrupt
2022-12-15 12:43 AM
Hello,
we are very interested by the fix you found.
Would you please communicate on it ?
Best Regards.
2022-12-15 6:18 AM
I managed to resolve the issue by replacing the original "spc5xx_serve_rxi_interrupt" driver (inside serial_lld.c) with this one:
static void spc5xx_serve_rxi_interrupt(uint32_t isdp) {
SerialDriver *sdp = (SerialDriver *) isdp;
uint16_t sr = sdp->linflexlp->UARTSR.R;
sdp->linflexlp->UARTSR.R = (uint16_t)(SPC5_UARTSR_NF | SPC5_UARTSR_DRF | SPC5_UARTSR_PE0);
if ((sr & SPC5_UARTSR_DRF) == SPC5_UARTSR_DRF) {
if(sdp->config->api_mode != SPC5_LIN_API_MODE_BUFFERED_IO) {
*sdp->rx_buf = (uint8_t)sdp->linflexlp->BDRM.B.DATA4;
//sdp->rx_buf++; // opistara 2021-02-17
sdp->linflexlp->UARTSR.R = (uint16_t)SPC5_UARTSR_RMB;
//sdp->rx_len--; // opistara 2021-02-17
sdp->rx_len = 0; // opistara 2021-02-17
if (sdp->rx_len == 0UL) {
//sdp->linflexlp->UARTCR.B.RXEN = 0; // opistara 2021-02-17
//sdp->linflexlp->LINIER.B.DRIE = 0; /* Interrupts disabled. */ // opistara 2021-02-17
if (sdp->linflexlp->UARTCR.B.TXEN == 0UL) {
sdp->linflexlp->LINIER.R &= ~((uint16_t)(SPC5_LIN_INTERRUPTS));
}
/* Call the related callback.*/
if (sdp->config->rx_end_cb != NULL){
sdp->config->rx_end_cb(sdp);
}
SPC5_LIN_RX_DONE(sdp);
}
} else {
*sdp->rx_write_ptr = (uint8_t)sdp->linflexlp->BDRM.B.DATA4;
sdp->rx_write_ptr++;
if (sdp->rx_write_ptr == sdp->rx_end_ptr) {
sdp->rx_write_ptr = sdp->rx_buffered_io;
}
if (sdp->rx_write_ptr == sdp->rx_read_ptr) {
sdp->rx_read_ptr++;
if (sdp->rx_read_ptr == sdp->rx_end_ptr) {
sdp->rx_read_ptr = sdp->rx_buffered_io;
}
}
}
}
}
and it worked very well for me.
Regarding the configuration "serial_config_UART", I used this one:
SerialConfig serial_config_UART = {
115200,
SD_MODE_8BITS_PARITY_NONE,
SPC5_LIN_API_MODE_ASYNCHRONOUS,
tx_callback,
rx_callback,
FALSE,
NULL,
0,
NULL
};
I hope that this will help you!
Regards,
Simone
2022-12-15 6:36 AM
Tante Grazie Simone,
I will report your fix to R&D Team.
Best Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.