2015-08-08 5:27 AM
Hi
I want to use External IRQ Pins for Wake up , Can Use These interrupts or not ? ex : EIRQ0 Best Regards Nazerian Vanima2015-08-09 10:00 PM
Hello,
Which power down mode you are using? Based on power down mode used, the exit sources are different. Refer section #8.1.3 of reference manual.As for using external interrupt, you need to use wakeup module (corresponding wakeup pin) for exiting the stop and standby power down mode.Regards,Mike.2015-08-09 10:41 PM
Hi Mike
Thanks for your response I use the STANDBY mode for going to sleep and use wake up pins for gonig to DRUN mode but my problem is the SPC560B50L5 have 19 Wakeup pins and i need 25 Wakeup pin because of this issue i think about external interrup . according to Refrence manual i think the MCU did'nt wakeup with external interrupt Best Regards Nazerian Vanima2015-08-09 10:49 PM
Yes, wakeup is not possible with external interrupt pins. Instead you can try some decoding logic using available wakeup pins.
Best Regards,Mike.2015-08-10 7:46 AM
Hello Vanima ,
From STANDBY mode, wakeup is not possible by EIRQ.you should use WKUP Interrupt. Best regards ErwanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.