2024-09-23 6:42 AM - last edited on 2024-09-23 7:04 AM by Peter BENSCH
Hi ST Team,
MCU is SPC584B70E1. CAN0 is used as ISR-Rx normally.
I want to choose "CAN FIFO 0 Rx New message Interrupt" as Wake-up Source.
In SPC5 Studio, I configurated on WKPU Configuration setting , I selected INT 0 as WakeUp Source and in the CAN setting FIFO is ENABLE vs.
Without wkpu_lld_start() and STOP0 Mode, CAN works expectedly. With Filtered IDs ISR_Rx_Buffer_Callback() executes, with the specific (Wake-Up message) packet FIFO_Rx_Callback() executes. But together with wake-up configuration does not works.
Is it possible to use "CAN FIFO 0 Rx New message Interrupt" as Wake-up Source??If it is ,how? On SPC5 IDE, How to configurate WKPU settings?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.