cancel
Showing results for 
Search instead for 
Did you mean: 

TESEO LIV4F low power

dl2
Associate

Hello, 

 

I am currently using the EVB-LIV4F and using page 8 of the UM3212 document to measure the current draw of the module. I am then placing it into SW-standby mode by sending the $PSTMFORCESTANDBY,<seconds>,1 command that I found on this post: https://community.st.com/t5/gnss-positioning/teseo-liv4f-wakeup-interrupt-and-nreset-confusion/td-p/615973

 

Under these conditions, I am measuring 0.0mV on the VCC (pin #9) and PM_VCC (pin #10) pins and 9.1mV on the VBAT (pin #7) and PM_VBAT (pin #8) pins. From the conversion given, the GNSS module is drawing 91uA on VBAT and not the advertised 10uA. 

Does the evaluation board need to be in a specific configuration to achieve the 10uA? Any jumpers that need to be added/removed?

Where is the documentation on the placement of jumpers? The eval board silkscreen does not have all jumpers labelled (Jxxx) and neither does UM3212 section 6.2... 

2 REPLIES 2
GalaxyQuest
ST Employee

Hi,

We are looking into this and will get back. Have you tried switching off Vcc supply when in standby?


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Franck_LMS
ST Employee

The command is $PSTMFORCESTANDBY,<seconds>. Remove the ",1" at the end.

On my EVB I have then 3.5mV and 35uA.
Then, switch OFF VCC : remove J508 and then I have 0.5mV and 5uA on VBAT.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.