Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Procedure to receive data from UART with ISR mode in SPC560P50L5?

Hi Technical team,Hardware Environment : SPC560P50L5I am using example program 'SPC560Pxx_RLA SERIAL Test Application for Discovery'I am able to transmit data to console window by using above example (using UART).I dont know , how to use this example...

RatheeshT by Associate II
  • 1347 Views
  • 1 replies
  • 0 kudos

Resolved! SPC560B54- DIS JTAG Error with External Device Programming

Trying to program SPC560B50L5 MCU with SPC560B54- Discovery board through JTAG.About 4 devices of discovery boards have No Target Error. Need to know is there any problem with debugger or the software's used or the MCU board.Complier used SPC5 Studi...

0693W000008xk3uQAA.jpg
$AK by Associate III
  • 1434 Views
  • 1 replies
  • 0 kudos

Resolved! Debugg and program SPC572L

We have the SPC572L -DISP dicovery board and the SPC5-UDESTK pluged in to the JTAG connector. When running UDE STK 5.2 our board is not avalible when selecting Target configuration. How can we get the connection to work?When will the SPC5 studio int...

Larsa by Associate III
  • 1901 Views
  • 2 replies
  • 0 kudos

Resolved! How to modify UTEST DCF Client?

Hello! I've tried to modify UTEST DCF Client but some questions (below) appeared to me.In RM0349 on the page 260 I see the it's Reset value. How can I read it? UTEST Flash memory with the address 0x00400308 is empty. At the same table I see "offset" ...

Mannhof by Associate II
  • 4686 Views
  • 5 replies
  • 0 kudos

Resolved! How to program SPC560B50L5 MCU

Using SP560B50 MCU, but programming the IC is the complex part.We used SPC560B54-DIS board to program the B50 IC, but the DIS board repeatedly fails with FDTI driver issue.Kindly suggest any other programmer or way to program them.Regards,AK

$AK by Associate III
  • 1356 Views
  • 1 replies
  • 0 kudos