Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! ?

-

DKuma.3 by Associate II
  • 1117 Views
  • 1 replies
  • 0 kudos

Resolved! Firmware Updater SPC560BC Family

Hi i have a custom board with SPC560B50L3 that is in the  SPC560BC Family.There is no SPC560BC xx Firmware Updater Component.If i try to add it (with shw incompatible components) of course i have problem generation files.There is some alternative?Th...

Resolved! Cannot Program SPC584B via UDESTK, Is my FLASH broken?

I was able to program my SPC584B70E3 via UDESTK 5.0 and SPC5-UDESTK tool. After using it for a while I tried to build a Bootloader application. Now I cannot access the device and program it or erase it.When I try to flash something I get the pop-up e...

TUyar.1 by Associate
  • 1768 Views
  • 1 replies
  • 0 kudos

JTAG can't connect to target board

I newly get a SPC56B-Discovery board. I have installed the SPC5Studio and UDE STK 5.0 on my PC. I select an example project and build OK with SPC5Studio. Then I connect the board to PC with USB cable. The PC can recongnize "PLS USB JTAG Adapter for S...

jxin.1 by Associate
  • 2487 Views
  • 1 replies
  • 1 kudos

Resolved! SPC570S MCU running FreeRTOS freeze upon receiving CAN messages

Hi,I have a SPC570S MCU running FreeRTOS and is connected to a CAN bus. I came across an issue where the MCU freezes randomly, when there traffic in the CAN bus before is it switched on. Could someone help me in this matter. This happens randomly, an...

NBula.1 by Associate III
  • 2716 Views
  • 3 replies
  • 0 kudos

Interrupt preemption - FreeRTOS

Dear all,I’m developing a system firmware for an engine ECU on SPC58EC microcontroller using FreeRTOS and SPC5Studio.During the tests I worked on interrupt priority and in particular I tested the correct servicing order of interrupt according to the ...

AParm.1 by Associate II
  • 2157 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5 compiling MCS code for SPC572L

We have a project running with TIM input signal and ATOM outputs and are now trying to use the MCS, we have looked at the GTM DPLL Test application and done some modification to the MCS program. Are there any tricks or options needed to compile the M...

Larsa by Associate III
  • 3663 Views
  • 4 replies
  • 0 kudos