Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC584xx MCU Wakeup based on ADC

Hello,I am using SPC584xx MCU for an automotive application. One requirement in the project is to wake up the ECU when the analog voltage value read by the ADC crosses a threshold.Is this requirement possible to be implemented using SPC584xx MCU? Is ...

SKara.7 by Associate II
  • 1843 Views
  • 1 replies
  • 0 kudos

Resolved! Saradc configuration.

I'm having trouble configuring saradc , as shown in the attached figure. I'm working on core 2 while on core 0 there is a program already made using the GTM module. Is there any relationship? Any suggestions to fix the attached error? Thanks!!

EReis.1 by Associate
  • 1916 Views
  • 1 replies
  • 0 kudos

Problems encountered in the implementation of The PIT interrupt

Hello allI want to send some SPI command periodically in SPC560p40 Microcontroller, so I am trying to generate a periodic interrupt request using PIT. I take “SPC560Pxx_RLA PIT Test Application for Discovery�? as example and write my code as bellow:A...

0693W00000JOFsHQAX.jpg 0693W00000JOFrsQAH.jpg 0693W00000JOFrxQAH.jpg
Bgh.1 by Associate II
  • 3232 Views
  • 8 replies
  • 0 kudos

Resolved! SPC5x pinout

Hi, where can I find microcontroller pinout?I miss something? I can't find spc5 pinouts in datasheets, where are these resources?​Best regards​

GMG by Associate III
  • 2475 Views
  • 3 replies
  • 0 kudos

Bootloader and application issue with SWT component

Hi,I am working on SPC58NG84E7 bootloader. Everything works fine - I have BL code(at 0xFC0000) which jumps to the APP location 0xFD0000 after waiting for 10sec after startup and executes the code there. Both codes are without SWT.Issue - But when I a...

AVM by Associate III
  • 7674 Views
  • 21 replies
  • 0 kudos

[SPC58Nxx] GTM 344 and TOMs granuliarity?

Hallo Everyone,If I setup two TOM channels with the TOM module clocked at 100MHz: (10nSec)GTM clocked at 100MHzCMD.CFGU.EN_CLK0 = trueCMD.CFGU.CLK_DIV0 = 1TOM0 module enabledTOM0_4 source clock = CMU_FXCLK0TOM0_4 period = 10000TOM0_4 duty = 5000TOM0_...

CoolMo by Associate III
  • 1939 Views
  • 2 replies
  • 0 kudos

Flash Erase for SPC58NG84E7 is not working

Hello,I am working on the bootloader, trying to flash only 256 bytes. So, before flashing, erasing the block 0xFF0000. There is already some data in this block. But erase is not happenin, even if FlashErase() returns 0 and FlashCheckStatus() also giv...

0693W00000JNFt8QAH.png
AVM by Associate III
  • 10606 Views
  • 23 replies
  • 1 kudos