Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Functional Safety Manual for SPC57x and SPC58x?

Hello,we consider using SPC57x or SPC58x for our products. I did find Safety Manuals for STM8 and STM32 but non for SPC5x. I know the chapter in the Reference Manuals with explanations of the CRC, STCU2 ... modules but I'm missing a complete list/tab...

F71334 by Associate II
  • 2759 Views
  • 1 replies
  • 0 kudos

Resolved! SPC58 setting

What are the settings in the attached picture?When a can interrupt comes in, are you setting whether to receive it through core 2 or core 0?

hans536 by Associate III
  • 2915 Views
  • 2 replies
  • 0 kudos

SPC58 : This is a question about the spc58 CAN BUS.

Currently I am making a can gateway system.​After receiving the data through can interrupt, task send data periodically.​The problem is that sometimes strange values ​​are sent when sending.​For example, a value of 10 was being received, but other va...

hans536 by Associate III
  • 2400 Views
  • 1 replies
  • 0 kudos

Resolved! Facing issues with installation of Live monitor.

Downloadedd MCTK library and motor control live monitor came as a part of it.Post installation run, I can see Live monitor GUI as attached.Something is clearly wrong with GUI. Please help resolve this issue.

Sjosh.4 by Associate
  • 2733 Views
  • 2 replies
  • 0 kudos

Resolved! SPC58 4B Line: ErrorProblem: Acknowledgement error on can analyzer

Problem: Acknowledgement error on can analyzer We are able to get the transmit data on TxFIFO Registers for CAN channel 2 but hardware is unable to transmit the message on the CAN channel 2.   May I know what we can do to correct this problem asap? ...

_legacyfs_online_stmicro_images_0693W00000bl3NeQAI.png
AOliv.8 by Associate
  • 2157 Views
  • 1 replies
  • 0 kudos

Freeze at configuring ATOM 3-5

Hello,My goal is to figure out how to run 15 synchronized center aligned PWM. I am trying to configure GTM ATOM module at custom board with SPC58EE80E7 with SPC5 studio GTM component RLA. Whenever I try to enable ATOM 3, 4 or 5 MCU freeze at startup....

MBedl.1 by Associate II
  • 1394 Views
  • 0 replies
  • 1 kudos

Resolved! Why I can't set HOST_DEBUG_EN in TnDCM CR register on SR6P7G7C7? I use key 0xE0E05FE0 to unlock it, but bit doesn't change the value. External debugger is not connected.

I'm working with SR6P7G7C7 and I would like to start CoreSight trace from MCU without external tools. I configured Core0 ETM and TMC ETR, but trace doesn't start. I assume the problem is in TnDCM_CR register, I am not able to set HOST_DEBUG_EN. I use...