Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC574k-DISP Ethernet

Hello,Did anyone managed to get the SPC574Kxx_RLA Network Ping Test Application for Discovery example working for the SPC574k-DISP board ?Connected the P14 jumper according to the readme.txt but no reply to the ping messages. 

SPC58-EC with Flash programming

HelloI am try to apply flash code to my project but it shows strange behavior.If I run run the code without break, program gose unhandled exception2.If put some break points here, flash erase and flash program works well.Left: Just before enter the f...

otcagon_0-1706408217909.png otcagon_1-1706408251030.png otcagon_2-1706408297081.png
otcagon by Associate II
  • 2255 Views
  • 1 replies
  • 0 kudos

SPC564: access external RAM

Hi,I'm trying to access external RAM with my SPC564A80.But when I step thru my code, the execution stops (hangs), as soon as I try to load from ext. RAM.I've checked setting up the MMU and the CS, but couldn't improve the situation.What else should I...

Mp_Esp by Associate
  • 1020 Views
  • 0 replies
  • 0 kudos

RGM Shows Core Watchdog -CWD Reset issue SPC572Lxx.

Hi,I 've bootloader and Application code for the mention SPC52Lxx series, and in Bootloader code have checked the reset status cause. so I'm getting the Functional Reset and the bit its set as Core Watchdog (CWD in RGM_FES) .Due to this its not jumpi...

ritesh07 by Associate
  • 1104 Views
  • 0 replies
  • 0 kudos

L9908 how to enter normal mode?

Hello, I would like to ask how the L9908 chip enters the normal mode. I now read the register status, saying that I am in safe off mode, and the config unlock register cannot write values, the rest of the NSR registers can be read and written.  

chimeng_0-1707057344070.png chimeng_1-1707057392017.png
chimeng by Associate
  • 1149 Views
  • 0 replies
  • 0 kudos

Wake up from STANDBY0 and HALT0 mode in SPC58EC80 eval board

How to wake up from STANDBY0 mode and also Halt0 mode?Is it possible to wake up or come out of STANDBY0 mode by pressing the reset button on the eval board?I tried it that way, but it is responding to the reset.As mentioned in the table above, can a ...

RSeba2_0-1706604928623.png
RSeba.2 by Associate III
  • 1088 Views
  • 0 replies
  • 0 kudos

SPC58xNxx PWM Generation with TOM (AN5552 Application Note)

Hello, on SPC58xNxx board, I've been trying to generate PWM signals using Timer Output Module (TOM) and I followed this guideline:AN5552: https://www.st.com/resource/en/application_note/dm00730101-generate-pwm-signals-with-gtm-stmicroelectronics.pdf ...

Resolved! SPC58EC-DISP - Gerber Files

Hello,I am looking for Gerber files of the SPC58EC-DISP boardIn the CAD resources folder I could find just the schematic, BOM and Layout in a .pdf file.https://www.st.com/en/evaluation-tools/spc58ec-disp.html#cad-resourcesBest regards